| Module 5 - Limits and Infinity |
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Lesson 4 | Self-Test |
| Lesson 5.4: Nonlinear Asymptotes |
|
In this lesson you will examine a rational fraction with a nonlinear asymptote. Using propFrac( will be helpful in determining the equation of the nonlinear asymptote.
5.4.1 Use your TI-89 to rewrite the rational function
Click here for the answer.
5.4.2 What do the parts of the proper fraction tell you about the graph of
Provide graphical support for the answer to Question 5.4.2 by graphing the function in a large window and in a window near x = 2. The Wide View
The graph of
The Narrow View
The graph of
A Medium View
To show both the vertical and parabolic asymptotic behavior of
As you have seen, the choice of viewing window can dramatically affect the appearance of a function, and different windows should be used to illustrate different features. The best graph is one in which all significant features of a function are displayed or implied. Such a graph is called a complete graph. Two or more windows are often needed to illustrate a complete graph. |
| < Back | Next > |
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|