| Module 5 - Limits and Infinity |
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Lesson 4 | Self-Test |
| Lesson 5.2: Holes |
|
In lesson 5.1 you found the vertical asymptote of the rational function
Finding Asymptote Candidates A list of candidates for the vertical asymptotes of a rational function may be found by finding the zeros of the denominator of the function.
One of the zeros corresponds to the vertical asymptote x = 3. However, there is no asymptote at Holes vs Asymptotes When x = -2, the function is undefined but the limit of the function as x approaches -2 from the left and from the right is a single specific value. Therefore, there is a hole in the graph, and x = -2 is not a vertical asymptote. The zero -2 is the x-coordinate of a hole in the graph. The y-coordinate of the hole can be determined by evaluating the limit of the function as x approaches -2.
5.2.1 Evaluate
Displaying the Hole
In lesson 5.1 you graphed the function
There is no apparent hole shown in this window, but if you change the viewing window, the hole may be seen.
ZoomDec automatically changes the viewing window to [-7.9, 7.9] x [-3.8, 3.8]. In this window, the x-values are even tenths (..., -0.2; -0.1, 0, 0.1, 0.2,...) and the space between pixels is 0.1. But assuming that xres is set to the default value of 2 in the window screen, when you trace using the arrow keys the x-values change by 0.2. Because xres is set at 2, the TI-89 will calculate values for every other column of pixels. The hole still does not appear on this graph because the x-values used to draw the graph skip from x = -1.9 to x = -2.1 and x = -2 is not evaluated. Resetting xres You can modify the viewing window so the TI-89 calculates values for every column of pixels by changing the value of "xres" in the Window screen.
Now you should be able to see the tiny hole at
The choice of Window values will determine whether or not a hole in the graph of a function will actually be visible on the graphing screen.
5.2.2 Find the vertical asymptote and the hole in the graph of
|
| < Back | Next > |
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|