| Module 24 - Power Series |
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test |
| Lesson 24.3: Taylor Series |
|
In Lesson 24.2 you found Maclaurin series that approximate functions near x = 0. This lesson investigates how to find a series that approximates a function near x = a, where a is any real number. A Taylor Series Given a function f that has all its higher order derivatives, the series
is called the Taylor series for f centered at a. The Taylor series is a power series that approximates the function f near x = a.
The partial sum
Every Maclaurin series, including those studied in Lesson 24.2, is a Taylor series centered at zero. The Taylor Polynomial of ex Centered at 1 The second-order Taylor polynomial centered at 1 for the function f(x) = ex can be found by using a procedure similar to the procedure given in Lesson 24.2.
The coefficient of the term (x - 1)k in the Taylor polynomial is given by
The coefficients of the second-order Taylor polynomial centered at 1 for ex are f(1) = e f '(1) = e
So the second-order Taylor polynomial for ex centered at 1 is
The Taylor series for ex centered at 1 is similar to the Maclaurin series for ex found in Lesson 24.2. However, the terms in the Taylor series have powers of (x - 1) rather than powers of x and the coefficients contain the values of the derivatives evaluated at x = 1 rather than evaluated at x = 0.
Graphing the function and the polynomial illustrate that the polynomial is a good approximation near
The second-order Maclaurin polynomial you found in Lesson 24.2,
24.3.1 Find the second-order Taylor polynomial centered at 1 for the function f(x) = ln x. Graph this polynomial together with f(x) = ln x. Click here for the answer. Other Taylor Series The Taylor series for one function can be used to find a Taylor series for a related function.
The third-order Taylor polynomial centered at 1 for f(x) = ln x is
The derivative of f(x) = ln x is
24.3.2 Find the second-order Taylor polynomial for
The Taylor Series for cos x2 Other modifications of a Taylor series yield other Taylor-series. For example, replacing each x with x2 in the Taylor series for f(x) = cos(x) gives the Taylor series for g(x) = f(x2) = cos(x2).
|
| < Back | Next > |
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|