| Module 24 - Power Series | ||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||
| Lesson 24.2: Maclaurin Series | ||||||||||||
|
In Lesson 24.1 you explored several power series and their relationships to the functions to which they converge. In this lesson you will start with a function and find the power series that best converges to that function for values of x near zero. Approximating a Function Near x = 0
Suppose f is some function. A second-degree polynomial p(x) = ax2 + bx + c that satisfies p(0) = f(0), Let f(x) = ex and p(x) = ax2 + bx + c. Use the fact that f and p are equal at x = 0 to find the value of c.
If c = 1, the function and the polynomial have the same value at x = 0, so p(x) = ax2 + bx + 1. Using a similar procedure, set the first derivatives equal when x = 0 and solve for b.
If b = 1, the function and the polynomial will have the same slope at x = 0, so p(x) = ax2 + x + 1. Set the second derivatives equal when x = 0 and solve for a.
If a = 1/2, the function and the polynomial will have the same concavity at x = 0. Graphs of the Function and the Approximating Quadratic Polynomial
The parabola has the same value, the same slope, and the same concavity as y = ex when x = 0, and the quadratic polynomial is a good approximation for y = ex when x is near 0.
24.2.1 Create a table of values for f(x) = ex and p(x) = (1/2)x2 + x + 1 with TblStart = -1 and
Click here for the answer. The General Procedure for Finding Maclaurin Series The procedure for finding the coefficients of a power series that approximates a function near x = 0 is summarized below, where the function y = f(x) is to be approximated by the power series polynomial
The series found in this fashion is called the Maclaurin series for the function f. Maclaurin series are often useful for integrating functions that do not have elementary antiderivates, for solving differential equations, and for approximating functions by polynomials. Coefficients in a Maclaurin Series Letting f(k)(x) denote the kth derivative of f, it can be shown that in a Maclaurin series the coefficient of the term that contains the kth power of x is given by The table below shows the first four coefficients of the Maclaurin series for f(x) = ex.
Therefore, the Maclaurin series for ex is
The Maclaurin series above is more than an approximation of ex, it is actually equal to ex on the interval of convergence,
Every Maclaurin series is centered at x = 0, the interval of convergence is centered at x = 0, and the Maclaurin series values and the function values are very close near x = 0.
The partial sum
24.2.2 Find the fifth-order Maclaurin polynomial for y = ln(1 + x) and interpret the result. Click here for the answer. 24.2.3 Graph y = ln(1 + x) and the fifth-order polynomial from 24.2.2. Click here for the answer. |
||||||||||||
| < Back | Next > | ||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|