Entering Test Mode by Choosing Restrictions

Note: This applies to the TI-Nspire™ App for iPad® and the TI-Nspire™ CAS App for iPad® except where noted. If you already have a test code, you can use the Enter Test Code method.

1. Tap Test Mode and then Choose Test Mode Restrictions.

This will open the Test Mode Restrictions dialog box.

2. Select the Default Angle you wish to use. Available units are Degree and Radian.
3. Select the CAS Mode you wish to use. (TI-Nspire™ CAS App for iPad® only)
• On enables CAS functions and symbol manipulation.
• Exact Arithmetic enables exact results in terms of stacked fractions, p, and radicals ‡.
• Off disables CAS and exact results.
4. Tap the toggle switch to enable or disable each restriction as needed.

The Test Code will automatically update based on your selections.

Note: For a detailed list of restrictions, refer to Understanding Test Mode Restrictions.

5. Tap Next.
6. On the Confirm App Self-Lock prompt, tap Yes.

• Pre-existing clipboard data is deleted.
• A green title bar indicates that the software is in Test Mode. It displays the Exit icon, Undo/Redo icons, Clear Document icon, the CAS or Exact Arithmetic mode status (when appropriate), Test Code, time elapsed while in the test session, the Test Mode Information icon, and the Settings icon.