Education Technology

STEM – Science, Technology, Engineering and Mathematics are naturally entwined.  Activities provided in this section focus on: Scientific exploration, Inquiry based learning, Coding and Engineering using the TI-Innovator.  

Year 9: STEM Classroom ActivitiesDownload
TI-Innovator
E:\MediaFiles\4\2\F\{42F8D07A-C110-4A38-952D-CB63559CB3D4}Missing Image Default.jpg

Ranger Introduction

Have you ever wondered how a car reverse sensor works? In this activity you will build a reverse sensor that provides audible and visual signals when an object becomes too close.  
    Download5
    Binary Output

    Binary Output

    How is light used to send text, images or sound? In this activity students convert a text message into binary code using the ASCII character map, the binary code is then used to oscillate an LED on the TI-Innovator according to the strings of 1’s and 0’s corresponding to their text message. Even a relatively slow signal is difficult to read prompting students to consider the next stage of this project.
      Download30
      Exp_Data_Thumb

      Exploring the Depths with Uniform Motion

      Exploring the Depths with Uniform Motion is a project-based STEM activity that explores uniform motion and will engage your students in the engineering design process while using TI-Nspire™ technology and the TI-Innovator™ Hub.
        Download42
        /media library/Images/Activities/AUS-NZ/Missing Image Default

        Pet Car Alarm

        In this TI-Innovator™ STEM project, students are given the challenge to design a “smart” pet alarm that will cool the interior of a car and notify the owner if a pet has accidentally been left in a hot car.
          Download7