Education Technology

The Function Editor App

How do I change the color and appearance of a graph?

To show how to set up the graph of a function follow these steps. Here, the mode is set to FUNCTION and the default settings are assumed.

Enter an equation in the Y= editor.

1. Select the Function Editor icon

2. Press c.

3. Press | l ² + 6.

To set the line color in the Y= editor:

 

1. Press the left arrow key  to highlight the color and line style indicator.

2. Press =.

The spinner dialog displays.

3. Press the right arrow key  to select MAGENTA.

4. Press the down arrow key .

Note: The thick line style is the default. It can be changed by pressing the left arrow key  or the right arrow key .

5. Press the down arrow key  to highlight OK and then press = to save changes.

Learn more about the apps