| Module 21 - Sequences and Series | ||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||
| Lesson 21.3: Recursively Defined Sequences | ||||||||||||
|
This lesson investigates a sequence that is defined recursively by examining the graph of the sequence and looking at the associated table of values. Defining a Recursive Sequence A recursive sequence defines a term an using one or more of the previous terms of the sequence. Because each term is defined using previous terms, the first few terms of the sequence must be defined explicitly. Explore the recursive sequence shown below that defines each term of the sequence as twice the previous term, an = 2an - 1, and the first term of the sequence is 1. an = 2an - 1, for n = 2, 3, 4, 5,... a1 = 1 Graphing the Recursive Sequence Define the sequence in the Y= Editor.
The function notation u1(n - 1) represents the function value at n - 1. There is no multiplication sign between u1 and (n - 1). The initial value of the function must also be entered so that the calculator will have a value with which to evaluate the second term. Subsequent terms will be determined by using previously computed terms.
ui1 represents u(1), the first term of the sequence.
The graph suggests that the sequence gets large without bound as n approaches
Creating a Table of Values The divergence of the sequence can by supported by viewing a Table of values.
It appears from the table that this sequence is the sequence an = 2n. The sequence an = 2n is called the geometric sequence and it is divergent. Defining a Recursive Sequence Requiring Two Previous Values In the sequence investigated above, each term was defined as twice the value of the preceding term. Recursive sequences can also be defined using more than one preceding term. Explore the recursive sequence that defines each term as the sum of the two previous terms where the first two terms are 1 and 1.
The initial value ui1 is the list {1,1}, which represents the values of the first two terms. The symbols '{' and '}' are found above the parentheses.
21.3.1 Display the table and identify the sequence shown. |
||||||||||||
| < Back | Next > | ||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|