| Module 21 - Exponential Growth and Decay | ||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||
| Lesson 21.2: Newton's Law of Cooling | ||
|
In this lesson you will explore an application that is modeled using exponential decay. The model used is similar to the one explored in Lesson 21.1. Newton's Law of Cooling Sir Isaac Newton (1642-1716) discovered how a hot liquid cools to the temperature of its surroundings. The form of the equation that models the cooling situation is a modification of the differential equation explored in Lesson 21.1. In that lesson, the rate of change of the balance in the account was directly proportional to the balance at any time t: The differential equation that describes how a liquid cools has a similar form. To write the equation for the cooling problem, we need the following variables.
Newton's Law of Cooling describes the change in the liquid's temperature. It says that the rate of cooling of a liquid is proportional to the temperature difference between the liquid and its surroundings. That is,
where k is the constant of proportionality and
The Temperature Equation An equation that gives the temperature of the liquid at time t can be found by solving the differential equation given above with the initial condition that the temperature difference at t = 0 is Y0 = I - S. The solution has the form
Substituting Y = L - S and Y0 = B - S the equation can be solved for L. The result is an equation that gives the temperature of the liquid at time t.
L = (B - S)e-k · t + S Specific Solutions If the required data is available, here is one way that the model can be used.
A Cooling Example Suppose a cup of water was heated to a temperature of 65°C and placed in a refrigerator that had a temperature of 5°C. The water cooled to a temperature of 11°C in 30 minutes. Find the temperature of the water after 60 minutes. The equation for the model is L = (B - S)e-k · t + S. The Equation Solver can be used to find specific values for k and then for L, but the equation must first be changed to a form that has zero on one side of the equation. Subtracting the terms on the right side of the equation gives
Enter the equation in the Equation Solver.
Find the value of k by using the condition L = 11 when T = 30.
The value of k, the constant of proportionality, is approximately 0.0768. You can now determine the temperature of the liquid after 60 minutes by simply changing the value for time and solving for L.
After 60 minutes the water will be about 5.6°C. 21.2.1 A cup of water was heated to a temperature of 70°C and placed in a refrigerator that had a temperature of 8°C. The water cooled to a temperature of 14°C in 30 minutes. Find the temperature of the water after 60 minutes. Click here for the answer. |
||
| < Back | Next > | ||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|