| Module 14 - Optimization | |||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self Test | |||||||||
| Lesson 14.1: The Cone Problem | |||||||||
|
In this lesson you will explore finding the maximum possible volume of a cone that is made by removing a sector from a circular piece of paper. You will write a function for volume in terms of the length of the arc that is removed and use the zeros of the function's derivative to identify values that will be used to find the maximum volume. Problems that ask for maximum or minimum values are called optimization problems, and each solution usually requires a multi-step procedure. This procedure can often be summarized as follows:
It is easy to get involved in the individual steps and lose sight of this lengthy overall process. A graphing calculator can help you focus on the overall process by assisting with the individual steps. A graphing calculator can also make it possible to do more difficult problems that could not be done without using technology. The Cone Problem Suppose that a circular piece of paper has a radius of one unit. Removing a sector from the circular piece of paper and fastening together the remaining seams creates a cone. The following discussion will find the length of the arc of the removed sector that results in the cone of maximum volume. The maximum volume will also be found. Drawing the Diagrams Diagrams that represent the problem are shown below. The left illustration depicts the circular piece of paper with a sector removed and the right diagram illustrates the completed cone.
Volume of a Cone as a Function of Radius and Height The quantity to be maximized is the volume of the cone. If the cone's height is h and r is its radius, its volume is given by Suppose x represents the length of the arc removed. The variables r and h can each be written as functions of x and the volume can be written as a function of x, as well. Radius as a Function of x
Note that the circumference of the original circular piece is 2
Because 2
Solving the equation for r gives
Store the function for r in Y1.
Height as a Function of x Review the diagram of the cone shown below.
The equation h2 + r2 = 1, which is obtained from the Pythagorean theorem, can be used to define h as a function of r. Because h can be written as a function of r and r is a function of x, h can be written as a function of x. Because r(x) was entered into Y1 in the Y= editor, Y1 may be used to define the height function,
Volume as a Function of x Volume was originally defined as a function of both r and h. Because r is a function of x and h is a function of r, volume can now be defined as a function of x.
The radius of the cone is stored in Y1 and the height of the cone is stored in Y2. Store the volume function,
The Derivative of Volume with Respect to x Store the derivative of the volume function, which is stored in Y3, into Y4 using the nDeriv feature of the Math menu.
The Domain of the Function in the Problem
Because the length of the arc that is removed must be greater than or equal to 0 and less than or equal to the circle's circumference, 2
Extreme Values of the Function on [0, 2
Any extreme value of the function must occur at a critical point or an endpoint. These values include:
Once all critical points are found, the function may be evaluated at those values and at the endpoints to determine where the maximum occurs. Graphing the Function and Its Derivative The maximum volume and its relationship to the corresponding zero of the first derivative can be illustrated by viewing the graphs of the volume function and its derivative.
Based on the first derivative, there appears to be two points of interest:
The Zero of the Derivative
Maximum Volume
Although both are approximations, notice that the zero of the derivative is about the same as the x-value at the volume's maximum point. The length of the removed arc that maximizes the volume is approximately 1.15299 units and the maximum volume is approximately 0.403067 cubic units, as shown at the bottom of the screen above. Endpoint Values
Evaluate the volume function at the endpoints of the domain, 0 and 2
The endpoints are minimums because the cone cannot have negative volume. Conclusion
The endpoints do not yield a maximum. The function is zero at the two endpoints, and since it is positive at the only critical point, that point must be the absolute maximum. The maximum volume is about 0.403067 cubic units and it occurs when x
Using the Second Derivative The second derivative can often be used to justify whether a critical point is a local maximum or a local minimum by revealing the function's concavity at that point. No conclusion can be drawn if the second derivative is zero or undefined at the critical point. The table below summarizes the relationships among the value of the second derivative at a critical point, the concavity of the function at the critical point, and whether a local minimum or local maximum occurs at the critical point.
14.1.1 Use the second derivative test to show that the volume has a local maximum at the critical point found above. Click here for the answer. We found the maximum volume of a cone created by removing a sector and demonstrated the relationship between the first and second derivatives and the volume function. The approach used was graphical and numeric. The analytic approach for this problem is rather complicated. It might be difficult to keep the overall process in mind while dealing with the lengthy functions for the first and second derivative. Technology handled the derivatives and that allowed us to focus on the procedure described at the beginning of the lesson as well as the relationship between the volume function and its derivatives. |
|||||||||
| < Back | Next > | |||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|