| Module 14 - Answers |
| Lesson 1 |
| Answer 1 |
14.1.1
Because the second derivative is negative at the critical point x = 1.15299, the function has a local maximum there. |
|
|
|
|
| Lesson 2 |
| Answer 1 |
|
14.2.1
Change Y2 to 355 / (
|
|
|
|
|
| Lesson 3 |
| Answer 1 |
|
14.3.1 Change Y2 to 355 / (
|
|
|
|
|
| Self Test |
| Answer 1 |
|
The height is h = sin(x). |
| Answer 2 |
|
Since the rectangle is symmetric about x =
|
| Answer 3 |
|
|
| Answer 4 |
|
|
| Answer 5 |
|
Because the derivative is positive to the left of x
|
| Answer 6 |
|
The zero of the derivative on the interval
|
| Answer 7 |
|
From the graph it appears that the derivative is defined on the entire interval. The end points produce an area of 0 and x
|
|
|
|
©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy |