| Module 7 - Limits and Infinity | ||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Lesson 4 | Self-Test | ||||||||||||||||||||
| Lesson 7.3: Oblique Asymptotes | ||||||||||||||||||||
|
In Lesson 7.1 you found vertical and horizontal asymptotes of a rational function. In this lesson you will see an
Investigating Oblique Asymptotes You can make an oblique asymptote obvious by adjusting the Window values before graphing a function.
There appears to be a vertical asymptote at x = -2, which corresponds to the zero of the denominator in the rational function. However, there does not seem to be a horizontal asymptote. Displaying an Oblique Asymptote Although there is no horizontal asymptote, there is an important feature of this rational function as x gets large without bound in both the positive and negative directions that may not be obvious in the viewing window above.
In this window the graph appears to be a line with a small wiggle near the y-axis. This slanted line is an oblique asymptote for the rational function
Finding the Oblique Asymptote
You can find the equation of an oblique asymptote by converting the rational function to a polynomial plus a
A proper fraction is a rational expression in which the degree of the numerator is less than the degree of the denominator. An improper fraction is a rational expression in which the degree of the numerator is greater than or equal to the degree of the denominator. An improper fraction may be changed into a polynomial plus a proper fraction by dividing the numerator by the denominator. The quotient gives the polynomial, and the proper fraction is given by the remainder over the divisor.
The quotient is x - 4 and the remainder is 9. This means the rational function is the sum of a linear polynomial function x - 4 and a proper fraction
Since
The linear function y = x - 4 is an equation of the oblique asymptote. The Wide View Graphical support that y = x - 4 is an oblique asymptote is provided by graphing both the line y = x - 4 and the rational function in a [-100, 100, 10] x [-200, 100, 20] window.
For values of x with large magnitude, the graphs of the rational function and the line appear to coincide in this window. (You can check this using the Trace feature.) How the Graphs Differ The difference between the graphs of the function and the line can be seen by displaying them in a smaller window.
Notice that the appearance of the graph of a rational function is dramatically affected by the choice of window values. In a large viewing window the graph of the rational function
The Narrow View
Now compare the graphs of the original rational function and the proper fraction
Near the vertical asymptote at x = -2 the graph of the rational function
7.3.1 Discribe the graph and asymptotes of
|
||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||