| Module 7 - Answers | ||||
| Lesson 1 | ||||
| Answer 1 | ||||
|
7.1.1
The vertical asymptote appears to be at about x = 3. The horizontal asymptote appears to be at about y = 2. |
||||
|
|
||||
|
| ||||
| Answer 2 | ||||
|
7.1.2
As x approaches 3 from the left, the function values are negative with increasing magnitude. In other words,
As x approaches 3 from the right, the function values become larger without bound. In other words,
|
||||
|
|
||||
|
| ||||
| Answer 3 | ||||
|
7.1.3
The tables show that as the magnitude of the x-coordinates increase, the y-coordinates get closer to 2.
|
||||
|
|
||||
|
| ||||
| Lesson 2 | ||||
| Answer 1 | ||||
|
7.2.1
Since the limit exists, x = -2 is not a vertical asymptote, but rather the x-coordinate of a hole. The coordinates of the hole are
|
||||
|
|
||||
|
| ||||
| Answer 2 | ||||
|
7.2.2
Because
Because
|
||||
|
|
||||
|
| ||||
| Lesson 3 | ||||
| Answer 1 | ||||
|
7.3.1
Because
|
||||
|
|
||||
|
| ||||
| Lesson 4 | ||||
| Answer 1 | ||||
|
7.4.1
The rational function has a vertical asymptote at x = 2. The polynomial y = x2 - 8x - 15 is a nonlinear asymptote for the rational function and the function resembles
|
||||
|
|
||||
|
| ||||
| Self Test | ||||
| Answer 1 | ||||
| y = 0 | ||||
| Answer 2 | ||||
| x = -3, x = 1 | ||||
| Answer 3 | ||||
| x = -3 | ||||
| Answer 4 | ||||
| x = 1 | ||||
| Answer 5 | ||||
|
|
||||
| Answer 6 | ||||
|
[-10, 10, 1] x [-100, 100, 10] Xres = 2 |
||||
|
|
||||
|
©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy |