Modes

p

Use p to choose modes. Press $ # ! " to choose a mode, and < to select it. Press - or % Q to return to the Home screen and perform your work using the chosen mode settings.

Default mode settings are shown highlighted.

DEG   RAD   GRAD Sets the angle mode to degrees, radians, or gradians.

NORM   SCI   ENG Sets the numeric notation mode. Numeric notation modes affect only the display of results, and not the accuracy of the values stored in the unit, which remain maximal.

NORM displays results with digits to the left and right of the decimal, as in 123456.78.

SCI expresses numbers with one digit to the left of the decimal and the appropriate power of 10, as in 1.2345678…105 (which is the same as 123456.78).

Note: In some restricted environments (for example function table, data editor, and the % h menu), the TI-30XS MultiView™ calculator may display E instead of …10n.

ENG displays results as a number from 1 to 999 times 10 to an integer power. The integer power is always a multiple of 3.

Note: C is a shortcut key to enter a number in scientific notation format. The result displays in the numeric notation format set in mode.

FLOAT   0123456789 Sets the decimal notation mode.

FLOAT (floating decimal point) displays up to 10 digits, plus the sign and decimal.

0123456789 (fixed decimal point) specifies the number of digits (0 through 9) to display to the right of the decimal.

CLASSIC   MATHPRINT

CLASSIC mode displays inputs and outputs in a single line.

MATHPRINT mode displays most inputs and outputs in textbook format.

Examples of Classic and MathPrint modes

Classic mode

MathPrint mode

Sci

Sci

Float mode and answer toggle key.

Float mode and answer toggle key.

Fix 2

Fix 2 and answer toggle key.

Un/d

Un/d

Exponent example

Exponent example

Square root example

Square root example

Cube root example

Cube root example