Last Answer

% i

The most recently calculated result is stored to the variable Ans. Ans is retained in memory, even after the TI-30XS MultiView™ calculator is turned off. To recall the value of Ans:

• Press % i (Ans displays on the screen), or
• Press any operations key (T, U, and so forth) as the first part of an entry. Ans and the operator are both displayed.

Example

Ans

3 V 3 <

 

V 3 <

 

3 % c % i <