Home Screen

On the Home screen, you can enter mathematical expressions and functions, along with other instructions. The answers are displayed on the Home screen. The TI-30XS MultiView™ screen can display a maximum of four lines with a maximum of 16 characters per line. For entries and expressions of more than 16 characters, you can scroll left and right (! and ") to view the entire entry or expression.

In the MathPrint™ mode, you can enter up to four levels of consecutive nested functions and expressions, which include fractions, square roots, exponents with ^, Ê, ex, and 10x.

When you calculate an entry on the Home screen, depending upon space, the answer is displayed either directly to the right of the entry or on the right side of the next line.

Special indicators may display on the screen to provide additional information concerning functions or results.

Indicator

Definition

2nd

2nd function.

HYP

Hyperbolic function.

FIX

Fixed-decimal setting. (See Modes section.)

SCI, ENG

Scientific or engineering notation. (See Modes section.)

DEG, RAD, GRAD

Angle mode (degrees, radians, or gradians). (See Modes section.)

K

Constant feature is on.

L1, L2, L3

Displays above the lists in data editor.

The TI-30XS MultiView™ calculator is performing an operation.

º »

An entry is stored in memory before and/or after the active screen. Press # and $ to scroll.

³ ´

An entry or menu displays beyond 16 digits. Press ! or " to scroll.