2nd Functions

%

Most keys can perform two functions. The primary function is indicated on the key and the secondary function is displayed above it. Press % to activate the secondary function of a given key. Notice that 2nd appears as an indicator on the screen. To cancel it before entering data, press % again. For example, % b 25 < calculates the square root of 25 and returns the result, 5.