Canadian IC Information
|
Product Name |
IC |
|
TI-Nspire™ Navigator™ Wireless Cradle |
451E-TINAVWC2 |
|
TI-Nspire™ Navigator™ Access Point |
451F-TINAVAP2 |
|
TI-Nspire™ CX Wireless Network Adapter |
451E-TINAVWNA |
|
TI-Nspire™ CX Navigator™ Access Point |
451F-TINAVAP3 |
|
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
451F-TINAVWNA2 |
Industry Canada Statement:
This device complies with Industry Canada license-exempt RSS standard(s). Operation is subject to the following two conditions:
| 1. | This device may not cause interference, and |
| 2. | This device must accept any interference, including interference that may cause undesired operation of the device. |
To ensure compliance with Industry Canada requirements, (SAR limit is 1.6 W/kg averaged over one gram of tissue), these products have been evaluated and found compliant in accordance with Industry Canada RSS-102 with respect to the Safety Code 6 for Human Exposure to RF Fields. The highest SAR value reported under this standard during product certification when worn on the body:
|
Product Name |
SAR Value |
|
TI-Nspire™ Navigator™ Wireless Cradle |
0.562 W/kg |
|
TI-Nspire™ Navigator™ Access Point |
0.995 W/kg |
|
TI-Nspire™ CX Wireless Network Adapter |
0.994 W/kg |
|
TI-Nspire™ CX Navigator™ Access Point |
0.433 W/Kg |
|
TI-Nspire™ CX Navigator™ Wireless Network Adapter – v2 |
0.716 W/Kg |
Equipment (or its transmit antenna) that is installed outdoors is subject to licensing and not supported by the listed products.
More information may be found in RSS-102 (http://www.ic.gc.ca/eic/site/smt-gst.nsf/eng/sf01904.html) and in Canada’s Safety Code 6 (http://www.hc-sc.gc.ca/ewh-semt/pubs/radiation/radio_guide-lignes_direct-eng.php).
Under Industry Canada regulations, this radio transmitter may only operate using an antenna of a type and maximum (or lesser) gain approved for the transmitter by Industry Canada. To reduce potential radio interference to other users, the antenna type and its gain should be so chosen that the equivalent isotropically radiated power (e.i.r.p.) is not more than that necessary for successful communication.
The device for the band 5150-5250 MHz is only for indoor usage to reduce potential for harmful interference to co-channel mobile satellite systems.
Avis de l'Industrie canadienne :
Cet appareil est conforme aux normes RSS d’Industrie Canada applicables aux appareils exempts de licence. Le fonctionnement est soumis aux deux conditions suivantes :
| 1. | Cet appareil ne doit pas occasionner d’interférence et |
| 2. | Cet appareil doit accepter les interférences, y compris celles susceptibles d’en compromettre le fonctionnement. |
Pour assurer la conformité avec les exigences d’Industrie Canada, (la limite DAS est de 1,6 W/kg en moyenne pour chaque gramme de tissu), ces produits ont été évalués et jugés conformes à la norme RSS-102 d’Industrie Canada en ce qui concerne le code de sécurité 6 relatif à l’exposition des personnes aux champs de radiofréquences. Valeur DAS la plus élevée recommandée par cette norme lors de la certification de produit lorsqu’il est porté sur le corps :
|
Nom produit |
Valeur DAS |
|
Station de connexion sans fil TI-Nspire™ Navigator™ |
0,562 W/kg |
|
Point d’accès TI-Nspire™ Navigator™ |
0,995 W/kg |
|
Adaptateur réseau sans fil TI-Nspire™ CX |
0,994 W/kg |
|
Point d’accès TI-Nspire™ CX Navigator™ |
0,433 W/kg |
|
Adaptateur réseau sans fil TI-Nspire™ CX Navigator™ – v2 |
0,716 W/kg |
L’équipement (ou son antenne de transmission) installé en extérieur est soumis à des licences et n’est pas pris en charge par les produits répertoriés.
Pour obtenir plus d’informations, consultez la section RSS-102 (http://www.ic.gc.ca/eic/site/smt-gst.nsf/eng/sf01904.html) et le code de sécurité 6 canadien (http://www.hc-sc.gc.ca/ewh-semt/pubs/radiation/radio_guide-lignes_direct-eng.php).
Conformément aux réglementations d’Industrie Canada, cet émetteur radio peut fonctionner uniquement avec une antenne d’un type et d’un gain maximal (ou inférieur) approuvé pour l’émetteur par Industrie Canada. Dans le but de réduire les risques d’interférence radio pour les autres utilisateurs, il est nécessaire de choisir le type d’antenne et son gain de sorte que la puissance isotrope rayonnée équivalente (p.i.r.e.) ne dépasse pas l’intensité nécessaire à une communication satisfaisante.
L’appareil pour la bande de 5 150 à 5 250 MHz est conçu pour une utilisation en intérieur uniquement, afin de réduire le risque d’interférences nuisibles aux systèmes par satellite mobiles utilisant un même canal.