Education Technology

The Function Editor App

How do I change the zoom factor settings?

To change the zoom factor settings, follow the steps below.

The zoom factor settings affect the scale change for the x and y-axes upon a zoom in or zoom out command. The factors are set from the zoom memory menu.

  1. Press f.

  2. Press the right arrow key › to MEMORY and select 4: SetFactors...

  3. -XFact sets the factor to change the x-axis.

    -YFact sets the factor to change the y-axis.