EULA v1.0.0
TI-Innovator™ Hub更新软件 1.x 用于Windows®和Mac®
适用范围:本试用许可或单用户许可适用于在任何国家获得的用于Windows®和Mac®的TI-Innovator™ Hub更新软件,只要本协议中未对该软件提供其他特别的许可条款。
重要提示——在安装本产品包内软件程序之前请仔细阅读本协议(“本协议”)。通过安装或以其他方式使用本产品包内的软件程序,阁下即同意接受本协议条款的约束。如果阁下不认同本协议的条款,请将原包装连同其全部内容归还至购买地点以获得全额退款。产品包须在购买之日起14日内归还。
本产品包内的软件程序(“软件”)以及任何相关的文档资料(合称“电脑程序”)由德州仪器(“TI”)和/或下文所示的任何适用的第三方许可人(合称“许可人”)授予许可。所授许可的具体细节详述如下。
(1.1)阁下同意TI拥有与电脑程序相关的全部专有权利,阁下不得复制任何与电脑程序相关的想法或商业秘密,不得对软件进行反向工程、反向汇编、反向编译或分析(不论以何种方式),也不得使用任何其他技术获取源代码,除非对于获得必要信息以达成与某个独立创作电脑程序的互用性而言,此等行为必不可少,且须基于以下前提条件:(1)此等行为由阁下履行或他人代表阁下履行,(2)为达成互用性所需的信息在阁下提出请求后的合理时间内TI未能向阁下提供,以及 (3)此等行为仅限于软件中为达成互用性所必需的部分。由此获得的信息仅可供阁下为达成互用性而使用。倘若阁下违反上述规定或尝试可能构成违反上述规定的任何行为,TI有权因具备充分理由而终止本协议并立即生效。阁下承认:对于任何违反或威胁违反本协议的行为而言,损害赔偿可能并不构成充分的救济,因此除了法律或衡平法下可获得的任何其他救济外,TI还有权就阁下或任何其他方的违约或威胁违约行为而寻求强制履行或禁止令救济(视情况而定)。
(1.2)阁下不得向第三方再分发、出租或以其他方式向第三方临时转让全部或部分的电脑程序或其任何复制件。阁下可将电脑程序出售,但须责成购买方以书面形式确认本协议中的许可条款对其具有约束力,并且阁下不得留存电脑程序的任何复制件。
(2)出现缺陷时的有限权利主张
(2.1)除非本协议中另行规定,否则若在下文(2.5)款所规定的时效期间内电脑程序出现风险转移时即存在的缺陷,TI将自行承担费用并选择为阁下维修缺陷或更换产品(“后续履行”)或取回电脑程序并向阁下退回购买价款。实施后续履行并不承担法律义务。在提起有关质保的权利主张时,阁下须出示购买凭证。
(2.2)如果电脑程序与相关用户指南中所描述的功能规格不符,则表明电脑程序出现缺陷。
(2.3)对于因过失、误用或不当处理而造成的任何缺陷,TI不承担任何责任,此等过失、误用或不当处理包括不当安装、操作、使用、维护或测试,用于TI明确界定以外的其他运用领域和环境条件;以及擅自与未经TI为此批准的其他产品结合使用,或者以任何方式对电脑程序进行修改或变更。
(2.4)如果后续履行在合理时间内不成功,即使阁下已提出损害赔偿的权利主张(该主张受制于下文的“责任限制”条款),阁下仍有权解除本协议或要求降价。
(2.5)与质保相关的权利主张的时效期间为一(1)年。对于维修后的电脑程序,原时效期间余下的时间将从经维修的电脑程序归还阁下之时继续计算。对于更换的电脑程序,时效期间应从经更换的电脑程序交付阁下之时重新计算。
(2.6)如果对被指的缺陷进行分析后表明无缺陷存在,TI有权按其当时适用的费率收取故障分析费。在此情况下,阁下还应承担电脑程序的运输费用和风险。
(3)知识产权赔偿、所有权瑕疵
(3.1)受制于下文(3.2)和(3.3)款以及责任限制条款,并且在质保权利主张的时效期间内(见上文“出现缺陷时的有限权利主张”条款的(2.5)款),对于最终裁定由阁下承担的或经TI同意作为和解或妥协的任何损害赔偿金、责任或费用,TI将对阁下进行赔偿,只要此等权利主张所基于的指控是电脑程序直接侵犯了美国、加拿大、日本、瑞士、中国大陆、香港特别行政区、台湾或欧盟成员国的任何专利、版权或其他知识产权;并且还须满足以下条件:(i)TI被及时告知该等权利主张,在适用情况下还应向其提供一份诉状,(ii)阁下所占有的全部证据均向TI提供,(iii)在针对该等权利主张的抗辩中(TI有权但无义务进行抗辩)以及为达成和解或妥协而进行的一切磋商中,阁下向 TI提供合理协助以及对此等活动的全权控制,并且(iv)阁下未向第三方承认存在知识产权的侵权行为。如果阁下为了减少损失或其他重要原因而停止使用电脑程序,阁下有义务向第三方权利要求人指出阁下不再使用并不构成对侵犯该第三方知识产权的承认。
(3.2)如果发生某种指控且TI因此有义务依照上述(3.1)款赔偿阁下,TI应视其选择采取以下措施:(i)获得允许阁下继续使用电脑程序的许可,或(ii)替换或修改电脑程序,使其不再侵权,所采用的方式不得对电脑程序的功能产生重大影响,或(iii)如果TI以商业上合理的开支无法实施(i)和(ii)项措施,则向阁下返还电脑程序的购买价款以及运费。如果TI选择上述第(iii)项措施,阁下应将仍为阁下占有、保管或控制的任何及所有产品归还给TI。除按下文“责任限制”条款提起的限制性损害赔偿主张之外,上述措施是TI承担的唯一责任。
(3.3)对于因阁下的故意而导致的任何费用、损失或损害赔偿,或者阁下未经TI事先书面同意而擅自达成的任何和解或妥协,TI不承担任何责任。只要侵权指控是基于以下情况,TI无义务进行抗辩,也不对任何费用、损失或损害赔偿承担责任:(1)阁下对电脑程序的使用结合了任何其他产品、软件或设备;(ii)阁下对电脑程序的使用方式或运用领域并非TI指定或希望的,不论TI是否知道或者阁下是否告知了TI此等方式或运用领域(除非TI已书面批准此等方式或运用领域);或(iii)阁下对电脑程序进行了修改(上述第(i)至(ⅲ)项所指的行为将使TI有权向阁下提起各项权利主张,此等权利主张在本协议中单称或合称为“其他权利主张”)。
(3.4)只要任何权利主张是基于其他权利主张而引起的指控,对于最终裁定由TI承担的或阁下同意作为和解或妥协的任何损害赔偿金、责任或费用,阁下应对TI进行赔偿,使其免受损害,并且对于向TI提起的任何此等权利主张,阁下将进行抗辩。
(3.5)本条述及知识产权侵权情况下TI所负的唯一责任以及阁下所享的唯一救济。
(4)责任限制
(4.1)对于因重大过失以及故意所造成的损害,许可人应承担不受限制的责任。任何进一步的许可人责任特此予以排除。许可人也不对因使用电脑程序而造成的或者阁下或任何其他方所遭受或发生的任何损害或损失(包括但不限于特殊、直接、间接、附带或后果性损害或者利润损失)承担责任,即使许可人已被告知发生此等损害或损失的可能性。
(4.2)除非是产品责任法项下的责任,否则有关违反电脑程序质量保证的行为,或以欺诈方式隐藏的缺陷,以及对人身或健康造成的伤害,上述责任限制适用于一切要求损害赔偿的权利主张,不论其法律依据为何。
(4.3)如果阁下针对许可人的员工或代理提起权利主张,上述责任限制同样适用。
一般规定
(1)如果阁下未能遵守本协议条款,TI可因具备充分理由而终止本协议并立即生效。本协议终止时,阁下同意将阁下所占有的电脑程序的原包装以及全部或部分复制件一并归还或销毁,并以书面形式向TI加以证明。
(2)电脑程序的出口以及再出口应遵守阁下购买电脑程序许可所在国的出口管制法律以及美国1969年的出口管理法(以修订后为准)。阁下有责任遵守此等法规。阁下同意:未经阁下购买电脑程序许可所在国的主管部门和/或美国商务部工业安全局的正式书面同意或许可(如果要求的话),阁下不拟亦将不会直接或间接地将电脑程序或技术数据出口、再出口或传播到阁下购买电脑程序所在国或美国相关法律法规限制对其进行此等出口、再出口或传播的任何国家。
(3)本协议受瑞士法律管辖并按其解释。不适用《联合国国际货物销售合同公约》。
(4)如果本协议的任何条款或任何条款之部分无效或成为无效,其余条款以及该条款之其余部分仍应保持其有效性。
(5)本协议构成阁下和TI之间的全部协议与谅解。对本协议的任何添加或修改必须采用书面形式并经TI正式授权的代表签署。该规定也适用于对书面形式这一要求的弃权。
(6)生产商是位于美国德克萨斯州达拉斯市的德州仪器(其详细地址为:12500 TI Blvd. Dallas, Texas 75243, U.S.A)。
****************************************************
The following components are covered by and distributed under the Apache License. Additional files and licenses follow the Apache 2.0 License.
Open Sans
Log4net
Swift 3 (Mac® only)
Apache License
Version 2.0, January 2004
http://www.apache.org/licenses/
TERMS AND CONDITIONS FOR USE, REPRODUCTION, AND DISTRIBUTION
1. Definitions.
"License" shall mean the terms and conditions for use, reproduction, and distribution as defined by Sections 1 through 9 of this document.
"Licensor" shall mean the copyright owner or entity authorized by the copyright owner that is granting the License.
"Legal Entity" shall mean the union of the acting entity and all other entities that control, are controlled by, or are under common control with that entity. For the purposes of this definition, "control" means (i) the power, direct or indirect, to cause the direction or management of such entity, whether by contract or otherwise, or (ii) ownership of fifty percent (50%) or more of the outstanding shares, or (iii) beneficial ownership of such entity.
"You" (or "Your") shall mean an individual or Legal Entity exercising permissions granted by this License.
"Source" form shall mean the preferred form for making modifications, including but not limited to software source code, documentation source, and configuration files.
"Object" form shall mean any form resulting from mechanical transformation or translation of a Source form, including but not limited to compiled object code, generated documentation, and conversions to other media types.
"Work" shall mean the work of authorship, whether in Source or Object form, made available under the License, as indicated by a copyright notice that is included in or attached to the work (an example is provided in the Appendix below).
"Derivative Works" shall mean any work, whether in Source or Object form, that is based on (or derived from) the Work and for which the editorial revisions, annotations, elaborations, or other modifications represent, as a whole, an original work of authorship. For the purposes of this License, Derivative Works shall not include works that remain separable from, or merely link (or bind by name) to the interfaces of, the Work and Derivative Works thereof.
"Contribution" shall mean any work of authorship, including the original version of the Work and any modifications or additions to that Work or Derivative Works thereof, that is intentionally submitted to Licensor for inclusion in the Work by the copyright owner or by an individual or Legal Entity authorized to submit on behalf of the copyright owner. For the purposes of this definition, "submitted" means any form of electronic, verbal, or written communication sent to the Licensor or its representatives, including but not limited to communication on electronic mailing lists, source code control systems, and issue tracking systems that are managed by, or on behalf of, the Licensor for the purpose of discussing and improving the Work, but excluding communication that is conspicuously marked or otherwise designated in writing by the copyright owner as "Not a Contribution."
"Contributor" shall mean Licensor and any individual or Legal Entity on behalf of whom a Contribution has been received by Licensor and subsequently incorporated within the Work.
2. Grant of Copyright License. Subject to the terms and conditions of this License, each Contributor hereby grants to You a perpetual, worldwide, non-exclusive, no-charge, royalty-free, irrevocable copyright license to reproduce, prepare Derivative Works of, publicly display, publicly perform, sublicense, and distribute the Work and such Derivative Works in Source or Object form.
3. Grant of Patent License. Subject to the terms and conditions of this License, each Contributor hereby grants to You a perpetual, worldwide, non-exclusive, no-charge, royalty-free, irrevocable (except as stated in this section) patent license to make, have made, use, offer to sell, sell, import, and otherwise transfer the Work, where such license applies only to those patent claims licensable by such Contributor that are necessarily infringed by their Contribution(s) alone or by combination of their Contribution(s) with the Work to which such Contribution(s) was submitted. If You institute patent litigation against any entity (including a cross-claim or counterclaim in a lawsuit) alleging that the Work or a Contribution incorporated within the Work constitutes direct or contributory patent infringement, then any patent licenses granted to You under this License for that Work shall terminate as of the date such litigation is filed.
4. Redistribution. You may reproduce and distribute copies of the Work or Derivative Works thereof in any medium, with or without modifications, and in Source or Object form, provided that You meet the following conditions:
-
You must give any other recipients of the Work or Derivative Works a copy of this License; and
-
You must cause any modified files to carry prominent notices stating that You changed the files; and
-
You must retain, in the Source form of any Derivative Works that You distribute, all copyright, patent, trademark, and attribution notices from the Source form of the Work, excluding those notices that do not pertain to any part of the Derivative Works; and
-
If the Work includes a "NOTICE" text file as part of its distribution, then any Derivative Works that You distribute must include a readable copy of the attribution notices contained within such NOTICE file, excluding those notices that do not pertain to any part of the Derivative Works, in at least one of the following places: within a NOTICE text file distributed as part of the Derivative Works; within the Source form or documentation, if provided along with the Derivative Works; or, within a display generated by the Derivative Works, if and wherever such third-party notices normally appear. The contents of the NOTICE file are for informational purposes only and do not modify the License. You may add Your own attribution notices within Derivative Works that You distribute, alongside or as an addendum to the NOTICE text from the Work, provided that such additional attribution notices cannot be construed as modifying the License.
You may add Your own copyright statement to Your modifications and may provide additional or different license terms and conditions for use, reproduction, or distribution of Your modifications, or for any such Derivative Works as a whole, provided Your use, reproduction, and distribution of the Work otherwise complies with the conditions stated in this License.
5. Submission of Contributions. Unless You explicitly state otherwise, any Contribution intentionally submitted for inclusion in the Work by You to the Licensor shall be under the terms and conditions of this License, without any additional terms or conditions. Notwithstanding the above, nothing herein shall supersede or modify the terms of any separate license agreement you may have executed with Licensor regarding such Contributions.
6. Trademarks. This License does not grant permission to use the trade names, trademarks, service marks, or product names of the Licensor, except as required for reasonable and customary use in describing the origin of the Work and reproducing the content of the NOTICE file.
7. Disclaimer of Warranty. Unless required by applicable law or agreed to in writing, Licensor provides the Work (and each Contributor provides its Contributions) on an "AS IS" BASIS, WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied, including, without limitation, any warranties or conditions of TITLE, NON-INFRINGEMENT, MERCHANTABILITY, or FITNESS FOR A PARTICULAR PURPOSE. You are solely responsible for determining the appropriateness of using or redistributing the Work and assume any risks associated with Your exercise of permissions under this License.
8. Limitation of Liability. In no event and under no legal theory, whether in tort (including negligence), contract, or otherwise, unless required by applicable law (such as deliberate and grossly negligent acts) or agreed to in writing, shall any Contributor be liable to You for damages, including any direct, indirect, special, incidental, or consequential damages of any character arising as a result of this License or out of the use or inability to use the Work (including but not limited to damages for loss of goodwill, work stoppage, computer failure or malfunction, or any and all other commercial damages or losses), even if such Contributor has been advised of the possibility of such damages.
9. Accepting Warranty or Additional Liability. While redistributing the Work or Derivative Works thereof, You may choose to offer, and charge a fee for, acceptance of support, warranty, indemnity, or other liability obligations and/or rights consistent with this License. However, in accepting such obligations, You may act only on Your own behalf and on Your sole responsibility, not on behalf of any other Contributor, and only if You agree to indemnify, defend, and hold each Contributor harmless for any liability incurred by, or claims asserted against, such Contributor by reason of your accepting any such warranty or additional liability.
END OF TERMS AND CONDITIONS
End of Apache License
****************************************************
The following components are covered by the Limited License agreement below.
Uniflash DebugServer and device support files
Uniflash Emulation components
TECHNOLOGY SOFTWARE PUBLICLY AVAILABLE
Copyright (c) 2016 Texas Instruments Incorporated
All rights reserved not granted herein.
Limited License Agreement.
This Limited License Agreement (“Agreement”) is a legal agreement between you (either an
individual or entity) and Texas Instruments Incorporated (“TI”). The “Software” consists of the
following materials: (a) the materials identified as TI proprietary software programs in the
software manifest for the software subject to the terms herein, and any “on-line” or electronic
documentation associated with these programs, or any portion thereof (the “Licensed
Materials”), and (b) the materials identified as open source materials or third party proprietary
software in the software manifest for the Software, or any portion thereof (“Public Software”).
For clarification, your use of the Licensed Materials is subject to the licensing terms contained in
this Agreement and your use of the Public Software is subject to the separate licensing terms
specified in the applicable software manifest and/or identified or included with the materials to
which they apply. This Agreement does not limit your rights under, or grant you rights that
supersede, the license terms of any applicable Public Software license agreement. By installing,
copying or otherwise using the Licensed Materials you agree to abide by the terms of this
Agreement. If you choose not to accept or agree with these terms, do not download or install
the Licensed Materials.
TI hereby grants you a world-wide, royalty-free, non-exclusive license under copyrights and
patents it now or hereafter owns or controls to make, have made, use, import, offer to sell and
sell ("Utilize") the Licensed Materials. With respect to the foregoing patent license, such license
is granted solely to the extent that any such patent is necessary to Utilize the Licensed Materials
alone. The patent license shall not apply to any combinations which include the Licensed
Materials, other than combinations with devices manufactured by or for TI (“TI Devices”). No
hardware patent is licensed hereunder.
Redistributions must preserve existing copyright notices and reproduce this Limited License
(including the above copyright notice and the disclaimer and (if applicable) source code license
limitations below) in the documentation and/or other materials provided with the distribution.
Redistribution and use in binary form, without modification, are permitted provided that the
following conditions are met:
*No reverse engineering, decompilation, or disassembly of this software is permitted with
respect to any software provided in binary form.
*any redistribution and use are licensed by TI for use only with TI Devices.
*Nothing shall obligate TI to provide you with source code for the software licensed and
provided to you in object code.
If software source code is provided to you, modification and redistribution of the source code are
permitted provided that the following conditions are met:
*any redistribution and use of the source code, including any resulting derivative works, are
licensed by TI for use only with TI Devices.
*any redistribution and use of any object code compiled from the source code and any
resulting derivative works, are licensed by TI for use only with TI Devices.
Neither the name of Texas Instruments Incorporated nor the names of its suppliers may be used
to endorse or promote products derived from this software without specific prior written
permission.
DISCLAIMER.
THIS SOFTWARE IS PROVIDED BY TI AND TI’S LICENSORS "AS IS" AND ANY EXPRESS
OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED
WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE
DISCLAIMED. IN NO EVENT SHALL TI AND TI’S LICENSORS BE LIABLE FOR ANY DIRECT,
INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
(INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN
ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE
POSSIBILITY OF SUCH DAMAGE.
END OF TERMS AND CONDITIONS
End of License
****************************************************