Funzionalità dell'app Impostazioni modalità
Impostazioni modalità di TI-84 Evo controlla il modo in cui vengono visualizzati numeri e grafici. Le impostazioni non vengono annullate quando si spegne la calcolatrice.
Dalla schermata iniziale seleziona l'icona Impostazioni modalità
oppure, dalla tastiera, premi j per accedere alla schermata delle impostazioni di modalità.
Premi la freccia giù ≥ o la freccia su ≤ per spostarti tra le diverse opzioni di impostazione; premi la freccia destra › e la freccia sinistra ‹ per spostare il cursore sulle impostazioni desiderate e premi =.
Per visualizzare le diverse impostazioni incluse nell'app Impostazioni modalità, consulta gli esempi riportati di seguito.
Change graph mode setting
Select Mode Settings icon
or press the j key.
- Change among Function, Parametric, Polar and Sequence modes.
Graphing modes define the graphing parameters.
Graph Icon changes depending on the Graph Type Mode Setting:
FUNCTION: graphing mode plots functions, where Y is a function of X.
PARAMETRIC: graphing mode plots relations, where X and Y are functions of T.
POLAR: graphing mode plots functions, where r is a function of θ.
SEQ: (SEQUENCE) graphing mode plots sequences. Three sequences are available: u, v, and w, with an option of the independent variables of n, n+1, and n+2.
Change to Graph Table view (split screen)
When a function is entered in the Y= editor, you can view a table of values by pressing a Ä.
Note: The table setup, a Ä, determines how table values are displayed. Check the table setup values if the table results are not in expected format of fraction. Using a mix of decimal and fractions will not retain fractions.
Change to Horizontal View (horizontal split screen)
In horizontal mode, the bottom zone can be the function editor, list editor, the table, or the calculator. The top area is always the graph screen. Change the bottom view by selecting the desired application using the icons on the home screen or the appropriate key.
Settings options
Mode settings with default settings highlighted:
| Setting | Result |
|---|---|
| MATHPRINT CLASSIC | Controls whether inputs/outputs are displayed as they are in textbooks. |
| NORMAL SCIENTIFIC ENG | Numeric notation setting. |
| FLOAT 0123456789 | Number of decimal places. |
| RADIAN DEGREE GRADIAN | Unit of angle measure. |
| FUNCTION PARAMETRIC POLAR SEQ | Type of graphing mode. |
| THICK DOT-THICK THIN DOT-THIN | Resets all Y= line styles. |
| SEQUENTIAL SIMULTANEOUS | Graphs draw in sequence or simultaneously. |
| REAL a+bi re^ (θi) | Real, rectangular complex, or polar complex number type. |
| FULL HORIZONTAL GRAPH-TABLE | Sets full screen or horizontal or vertical split-screen modes. |
| n/d Un/d | Display as a simple fraction or mixed number. |
| AUTO DECIMAL | Displays answers in similar format to input, a decimal, or fraction (as supported). |
| DIAGNOSTICS ON DIAGNOSTICS OFF | Determines which information is displayed in a statistical regression calculation (r, r², R²). |
| LANGUAGE | Select the language setting. Press ≥ or ≤ to move off the spinner to set the new language. |