DISCONNECT breaks the association between a specified control or sensor and the pin/port it is associated with. If the specified sensor or control is not currently connected to anything, an error is generated.
The DISCONNECT command does not generate an active response, other than possible error responses. Pins associated with an actively connected sensor, or control, are released from use and, in general, are set to a digital input state with no enabled pullup/pulldown.
DISCONNECT - disconnect something that has been connected, by index if needed.
Command: |
DISCONNECT-Input... |
---|---|
Command Syntax: |
DISCONNECT |
Range: |
|
Describe: |
Removes the association of a sensor or control with a pin, or set of pins, if such association exists. Places the pin(s) back to an INPUT state. |
Result: |
. |
Type or |
|
CE Calculators
|
TI‑Nspire™ CX
|