MAGNETIC

Command:

DISCONNECT MAGNETIC i

Command Syntax:

DISCONNECT MAGNETIC 1

Range

Describe:

The MAGNETIC sensor is used to detect the presence of a magnetic field. It uses the Hall effect. It is also known as a Hall effect sensor.

 

The DISCONNECT command removes the sensor from the program.

Result:

The name “MAGNETIC 1” is now disconnected from the sensor. It cannot be used in the program after a DISCONNECT command.

Type or
Addressable Component:

Sensor