| Module 23 - Parametric Equations | ||||||||||||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||||||||||||
| Lesson 23.2: Chain Rule for Parametric Equations | ||||||||||||||||||||||||||||||
|
This lesson investigates the procedure to find derivatives, such as
The Chain Rule Suppose a curve is defined by the parametric equations x = f(t) y = g(t)
The Chain Rule states that the derivative
Finding First and Second Derivatives
The procedure below will create two functions that return the values of
Use the new functions to find dy/dx and d2y/dx2 for the parametric equations x(t) = sec t y(t) = tan t
Define the parametric equations below. Recall that sec
Find
Finding Derivatives from a Graph The slope of the tangent line at a point on the graph of a parametric curve can be found by using the "Derivative" feature of the Math menu on the Graph screen.
The graph is a hyperbola and the diagonal lines are not a part of the graph. The two diagonal lines are similar to the vertical lines that often appear in graphs of functions that have vertical asymptotes.
You can use the "Derivatives" feature in the F5:Math menu on the Graph screen to find the value of
23.2.1 Find the value of
Finding the Equation of the Tangent Line
The tangent to the curve at the point when t = 0.5 is drawn and the equation of the tangent line is shown at the bottom of the screen. 23.2.2 Find the slope of the tangent line when t = 2 for the parametric equations
Click here for the answer. 23.2.3 Display the curve
Click here for the answer. |
||||||||||||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||||||||||||