| Module 22 - Differential Equations and Euler's Method | ||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||
| Lesson 22.3: Second-Order Differential Equations | ||||||||||||||||||||
|
In Module 20 you used EULERG and EULERT to solve first-order differential equations. In this lesson you will learn to use another program called DIFF2G to solve second-order differential equations. Defining a Second-Order Differential Equation A second-order differential equation contains a second derivative. For example, if y is the height above ground of a falling object then the first-order derivative y ' is the object's velocity and the second derivative y " is its acceleration. The equation y " = k is a second-order differential equation that represents the movement of an object that has constant acceleration k. Initial-value problems that involve a second-order differential equation have two initial conditions. Solving Elementary Second-Order Differential Equations Suppose that an object is dropped from a height of 48 feet. Because it is dropped without thrust, the initial velocity is zero. The only force acting on the object is gravity, which accelerates it downward 32 feet per second squared. If y is the height of the object above the ground at time t, then y ' is the velocity of the object and y " is its acceleration. The equation for the height of the object can be found by solving two first order differential equations. Because acceleration is the derivative of velocity, the second-order differential equation for acceleration, y " = a = -32, can be rewritten as a first-order differential equation.
Because velocity is the derivative of height, the equation for velocity v = 32t can be rewritten as a first order differential equation.
48 = -16 · 0 + C C = 48 The height of the object at time t is given by y = -16t2 + 48. Using The Solution The object's height above the ground at t = 1.3 seconds after it was dropped can be found by substituting t = 1.3 in y = -16t2 + 48. So the height of the object at t = 1.3 is 20.96 feet. Graphical and Numerical Solution The program DIFF2G can be used to find visual and numerical solutions to second-order differential equations without finding the analytic solution. The program takes a second-order differential equation like y " = h(x) and two initial conditions and produces graphs and tables-of-values for both y ' = g(x) and y = f(x). Downloading the Program to Your Computer
Transferring the Program to the TI-83 Click here to get information about how to obtain the needed cable and review the procedure to transfer the program from your computer to your calculator.
Using DIFF2G DIFF2G can be used to solve y " = 32 with initial conditions y(0) = 48 and y '(0) = 0.
After entering the step size, the program will take a few minutes to calculate the solution. When the calculations are complete you should see two graphs.
22.3.1 One of the graphs is height and the other is velocity. Which is which? Click here for the answer. The graph can be used to approximate the height at t = 1.3.
DIFF2G gives an approximation for y(1.3) of 20.752 feet. This is fairly close to the exact value of 20.96 feet found earlier in this lesson.
22.3.2 Approximate the velocity of the object just before it hits the ground by tracing on the height curve to the x-intercept then pressing
|
||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||