| Module 18 - The Fundamental Theorem | ||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||
| Lesson 18.2: Area Functions, A Visual Approach | ||||||
|
This lesson develops area functions using a visual approach by exploring the values of the areas under a curve when the right-hand endpoint changes. The concept is illustrated by graphing a definite integral in which the right-hand endpoint is variable. If a non-negative curve and a left-hand endpoint are given, an area function can be found for a right-hand endpoint that varies. It is necessary to distinguish between the independent variables for the curve function and for the area function. If x is used to denote the variable right-hand endpoint of the region, a second variable, t, could be used in the description of the curve function.
Letting x represent the right-hand endpoint, the area under the curve For example, if x = 3 the area under the curve between t = 1 and t = 3 is about 1.099, as illustrated in the screens below.
18.2.1 Use the Definite Integral command to find the areas under
Click here for the answer. 18.2.2 Make a scatter plot of your results and find the logarithmic regression (LnReg) equation that best fits the data. Graph this equation together with the scatter plot. Click here for the answer. Based on how closely the function fits the data, it appears that the area function may be the natural logarithmic function A (x) = ln x. Graphing Integrals
The procedure below will graph
The graph will be slow to appear because the calculator has to compute a new definite integral for each point it plots, but you should see the area function
Notice that the graph of A(x) appears to be the same as the graph of y = lnx, the regression equation we found above.
18.2.3 Based on these graphs, predict the function that is equal to
18.2.4 Describe how the Fundamental Theorem of Calculus applies. Click here for the answer.
Illustrating Suppose that you do not know a formula for the curve function but you have its graph. You can determine the shape of the area function by analyzing the graph of the curve.
Below is the graph of
Visualize the area under the graph of f being filled with thin rectangular sticks where the height of each stick is the y-value of the curve function. Each successive rectangular stick is shorter than the prior one. The Riemann sum is growing more slowly with each step as you move to the right because the area of each successive rectangle is less than the one before, as shown below. Therefore the area function is increasing at a decreasing rate. This means the area function is concave downward.
Using the Fundamental Theorem of Calculus The Fundamental Theorem of Calculus states that the derivative of the area function is the curve function. That means that the curve function values correspond to slopes of tangent lines of the area function. Some of the characteristics of the area function that can be determined from the graph of the curve function are listed below.
18.2.5 Examine the graph of f(x) between x = 0 and x = 4 shown below. Consider how the area function
Click here for the answer. |
||||||
| < Back | Next > | ||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||