Last Answer

% i

The most recently calculated result is stored to the variable ans. ans is retained in memory, even after the TI-34 MultiView™ calculator is turned off. To recall the value of ans:

• Press % i (ans displays on the screen), or
• Press any operations key (T, U, and so forth) as the first part of an entry. ans and the operator are both displayed.

Examples

ans

3 V 3 <

 

V 3 <

 

3 % c % i <