2nd Functions
%
Most keys can perform two functions. The primary function is indicated on the key and the secondary function is displayed above it. Press % to activate the secondary function of a given key. Notice that 2nd appears as an indicator on the screen. To cancel it before entering data, press % again. For example, 3 % c 125 < calculates the cube root of 125 and returns the result, 5.