Pi

g

p = 3.141592653590 for calculations.

p = 3.141592654 for display.

Example

p

2 V g <

 

n

³ Problem

What is the area of a circle if the radius is 12 cm?

Reminder: A = pr2.

g V 12 G 2 <

n

The area of the circle is 144 p square cm. The area of the circle is approximately 452.4 square cm when rounded to one decimal place.