Using Wizards

Some functions in the Catalog have a wizard that prompts you for each argument. Functions that have wizard support are identified with the wand symbol ().

To enable wizards

1. Tap to hide the TI-Nspire™ keyboard if it is showing.
2. Tap Utilities , and then go to Catalog. By default, the Tools Wizard is OFF.

3. Slide the button to the right to enable the Tools Wizard.
4. Select the function you want to insert. (The function must have wizard support.)
5. Tap Done.

The wizard opens and prompts for each argument before the function is inserted into the entry line.

6. Enter the arguments needed for the selected function.

Note: If the keyboard is needed to complete an entry, it opens when you tap the field.

7. Tap OK as needed to complete entries in each prompt for the selected function.

The selected function is inserted into the Calculator entry line.

Note: If a Catalog function requires a defined variable, you must define the variable before you can insert the Catalog item.