Defining Variables

Any portion or attribute of an object or function created within an application can be stored as a variable. Examples of attributes that can become variables include the:

• Area of a rectangle
• Radius of a circle
• Value contained in a spreadsheet cell
• Contents of a row or column in a spreadsheet
• Function expression

When you create a variable, it is stored in memory.

Types of Variables

You can store the data types listed in the following table as variables.

Data type

Examples

Expression

2.54

1.25E6

2p

(x-2)2

List

{2, 4, 6, 8}

{1, 1, 2}

{"red", "blue", "green"}

Matrix

This can be entered as: [1,2,3;3,6,9]

Character string

"Hello"

"xmin/10"

"The answer is:"

Function, program

myfunc( arg )

ellipse( x, y, r1, r2)

Measurement

area

perimeter

length

slope

angle