Education Technology

TI Connect™ Evo App Features

TI-Connect™ Evo is a web-based app that provides connectivity between a computer and a TI-84 Evo graphing calculator. It allows you to capture the calculator screen, transfer files to and from the calculator, and update the OS on the calculator.

System Requirements

  • Active internet connection
  • Web USB enabled
  • Access to shared memory, files, and clipboard

Note: For the latest hardware, operating system, browser, and other requirements, please visit the product page.

Supported Calculators

  • TI-84 Evo

To get started and explore the different pages of the app, see the examples below.

Getting started

1.    Open a compatible browser.
You may also Connect your TI-84 Evo calculator to the computer and click on TI-84 Evo detected pop up message - it will open the application in the default browser. If the default browser is compatible, then you may skip to step 4.

2.    Enter connectevo.ti.com into the address bar.
If prompted, click Agree and Proceed to accept cookies, and then click the ACCEPT button to agree with the TI terms and conditions.
A compatibility check will be performed while the app loads. If any issues are found, a page will display with information on what needs to be addressed.

3.    After the Let's Get Started page loads, connect your TI-84 Evo calculator to your computer.
Note: If your computer only has a USB-C port, you will need a USB-C to USB-C cable to connect your calculator.

4.   Click CONNECT TO CALCULATOR.

5.   On the popup window, click the name of your calculator and then click Connect.
The home page will open displaying the four available options: Capture Screen, Send Files, Install OS, and Exit Test Mode.

Navigating on the app

There are two ways to navigate on the TI Connect™ Evo app after connecting your calculator:

  • TI Connect™ Evo logo on the top left of each page which links to the home page
  • Links to each function on the top right of each page except the home and Let's Get Started pages

Note: If your calculator is disconnected and then reconnected (or you connect another calculator), you will be redirected to the Let's Get Started page.

Capturing the calculator screen

1.    Navigate to the CAPTURE SCREEN page.

2.    Click the CAPTURE SCREEN button.
The current calculator screen will display.
Note: To capture another screen, make the necessary changes on the calculator and click the CAPTURE SCREEN button again.

3.    Click one of the following buttons:

There are two actions a user can perform after capturing a screen:

  Copy to Clipboard: Copies the current screen to the computer clipboard so you can use the image in other apps.

  Save to Computer: Saves the current screen to your computer Downloads folder.

Sending files to or from the calculator

1.    Navigate to the SEND FILES page.

  • To send files from your computer to your calculator, click SEND TO CALCULATOR.
    This will open the file explorer where you can select the files from your computer to send to the calculator.
  • To send files from your calculator to the computer, select the file(s) you want to send, or use the check box to Select All, and then click SEND TO COMPUTER.

 

Installing or updating the OS

1.    Navigate to the INSTALL OS page.

2.    Click INSTALL OS.

3.   After reading the WARNING, click either the CANCEL or CONTINUE button.
Clicking CONTINUE will install the latest OS Update.

Exiting Test Mode

1.    Navigate to the EXIT TEST MODE page.

2.    Click the EXIT TEST MODE button.
A confirmation message will appear.