L

Lbl

Lbl labelName

Defines a label with the name labelName within a function.

You can use a Goto labelName instruction to transfer control to the instruction immediately following the label.

labelName must meet the same naming requirements as a variable name.

Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook.

lcm()

lcm(Number1, Number2) expression
lcm(List1, List2) list
lcm(Matrix1, Matrix2) matrix

Returns the least common multiple of the two arguments. The lcm of two fractions is the lcm of their numerators divided by the gcd of their denominators. The lcm of fractional floating-point numbers is their product.

For two lists or matrices, returns the least common multiples of the corresponding elements.

left()

left(sourceString[, Num]) string

Returns the leftmost Num characters contained in character string sourceString.

If you omit Num, returns all of sourceString.

left(List1[, Num]) list

Returns the leftmost Num elements contained in List1.

If you omit Num, returns all of List1.

left(Comparison) expression

Returns the left-hand side of an equation or inequality.

libShortcut()

libShortcut(LibNameString, ShortcutNameString
[, LibPrivFlag]) list of variables

Creates a variable group in the current problem that contains references to all the objects in the specified library document libNameString. Also adds the group members to the Variables menu. You can then refer to each object using its ShortcutNameString.

Set LibPrivFlag=0 to exclude private library objects (default)
Set LibPrivFlag=1 to include private library objects

To copy a variable group, see CopyVar on here.
To delete a variable group, see DelVar on here.

This example assumes a properly stored and refreshed library document named linalg2 that contains objects defined as clearmat, gauss1, and gauss2.

LinRegBx

LinRegBx X,Y[,[Freq][,Category,Include]]

Computes the linear regression y = a+bx on lists X and Y with frequency Freq. A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension except for Include.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Category is a list of numeric or string category codes for the corresponding X and Y data.

Include is a list of one or more of the category codes. Only those data items whose category code is included in this list are included in the calculation.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.RegEqn

Regression Equation: a+bx

stat.a, stat.b

Regression coefficients

stat.r2

Coefficient of determination

stat.r

Correlation coefficient

stat.Resid

Residuals from the regression

stat.XReg

List of data points in the modified X List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.YReg

List of data points in the modified Y List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.FreqReg

List of frequencies corresponding to stat.XReg and stat.YReg

LinRegMx

LinRegMx X,Y[,[Freq][,Category,Include]]

Computes the linear regression y = mx+b on lists X and Y with frequency Freq. A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension except for Include.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Category is a list of numeric or string category codes for the corresponding X and Y data.

Include is a list of one or more of the category codes. Only those data items whose category code is included in this list are included in the calculation.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.RegEqn

Regression Equation: y = mx+b

stat.m, stat.b

Regression coefficients

stat.r2

Coefficient of determination

stat.r

Correlation coefficient

stat.Resid

Residuals from the regression

stat.XReg

List of data points in the modified X List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.YReg

List of data points in the modified Y List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.FreqReg

List of frequencies corresponding to stat.XReg and stat.YReg

LinRegtIntervals

LinRegtIntervals X,Y[,F[,0[,CLev]]]

For Slope. Computes a level C confidence interval for the slope.

LinRegtIntervals X,Y[,F[,1,Xval[,CLev]]]

For Response. Computes a predicted y-value, a level C prediction interval for a single observation, and a level C confidence interval for the mean response.

A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension.

X and Y are lists of independent and dependent variables.

F is an optional list of frequency values. Each element in F specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.RegEqn

Regression Equation: a+bx

stat.a, stat.b

Regression coefficients

stat.df

Degrees of freedom

stat.r2

Coefficient of determination

stat.r

Correlation coefficient

stat.Resid

Residuals from the regression

For Slope type only

Output variable

Description

[stat.CLower, stat.CUpper]

Confidence interval for the slope

stat.ME

Confidence interval margin of error

stat.SESlope

Standard error of slope

stat.s

Standard error about the line

For Response type only

Output variable

Description

[stat.CLower, stat.CUpper]

Confidence interval for the mean response

stat.ME

Confidence interval margin of error

stat.SE

Standard error of mean response

[stat.LowerPred,
stat.UpperPred]

Prediction interval for a single observation

stat.MEPred

Prediction interval margin of error

stat.SEPred

Standard error for prediction

stat.y

a + bXVal

LinRegtTest

LinRegtTest X,Y[,Freq[,Hypoth]]

Computes a linear regression on the X and Y lists and a t test on the value of slope β and the correlation coefficient ρ for the equation y=α+βx. It tests the null hypothesis H0:β=0 (equivalently, ρ=0) against one of three alternative hypotheses.

All the lists must have equal dimension.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Hypoth is an optional value specifying one of three alternative hypotheses against which the null hypothesis (H0:β=ρ=0) will be tested.

For Ha: β0 and ρ0 (default), set Hypoth=0
For Ha: β<0 and ρ<0, set Hypoth<0
For Ha: β>0 and ρ>0, set Hypoth>0

A summary of results is stored in the stat.results variable. (See here.)

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

 

Output variable

Description

stat.RegEqn

Regression equation: a + bx

stat.t

t-Statistic for significance test

stat.PVal

Smallest level of significance at which the null hypothesis can be rejected

stat.df

Degrees of freedom

stat.a, stat.b

Regression coefficients

stat.s

Standard error about the line

stat.SESlope

Standard error of slope

stat.r2

Coefficient of determination

stat.r

Correlation coefficient

stat.Resid

Residuals from the regression

linSolve()

linSolve( SystemOfLinearEqns, Var1, Var2, ...) list

linSolve(LinearEqn1 and LinearEqn2 and ..., Var1, Var2, ...) list

linSolve({LinearEqn1, LinearEqn2, ...}, Var1, Var2, ... list

linSolve(SystemOfLinearEqns, {Var1, Var2, ...})  list

linSolve(LinearEqn1 and LinearEqn2 and ..., {Var1, Var2, ...}) list

linSolve({LinearEqn1, LinearEgn2, ...}, {Var1, Var2, ...})  list

Returns a list of solutions for the variables Var1, Var2, ...

The first argument must evaluate to a system of linear equations or a single linear equation. Otherwise, an argument error occurs.

For example, evaluating linSolve(x=1 and x=2,x) produces an “Argument Error” result.

ΔList()

ΔList(List1) list

Note: You can insert this function from the keyboard by typing deltaList(...).

Returns a list containing the differences between consecutive elements in List1. Each element of List1 is subtracted from the next element of List1. The resulting list is always one element shorter than the original List1.

listmat()

listmat(List [, elementsPerRow]) matrix

Returns a matrix filled row-by-row with the elements from List.

elementsPerRow, if included, specifies the number of elements per row. Default is the number of elements in List (one row).

If List does not fill the resulting matrix, zeros are added.

Note: You can insert this function from the computer keyboard by typing list@>mat(...).

ln()


ln(Value1) value
ln(List1) list

Returns the natural logarithm of the argument.

For a list, returns the natural logarithms of the elements.


If complex format mode is Real:


If complex format mode is Rectangular:

ln(squareMatrix1) squareMatrix

Returns the matrix natural logarithm of squareMatrix1. This is not the same as calculating the natural logarithm of each element. For information about the calculation method, refer to cos() on.

squareMatrix1 must be diagonalizable. The result always contains floating-point numbers.

In Radian angle mode and Rectangular complex format:

To see the entire result,
press 5 and then use 7 and 8 to move the cursor.

LnReg

LnReg X, Y[, [Freq] [, Category, Include]]

Computes the logarithmic regression y = a+bln(x) on lists X and Y with frequency Freq. A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension except for Include.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Category is a list of numeric or string category codes for the corresponding X and Y data.

Include is a list of one or more of the category codes. Only those data items whose category code is included in this list are included in the calculation.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.RegEqn

Regression equation: a+bln(x)

stat.a, stat.b

Regression coefficients

stat.r2

Coefficient of linear determination for transformed data

stat.r

Correlation coefficient for transformed data (ln(x), y)

stat.Resid

Residuals associated with the logarithmic model

stat.ResidTrans

Residuals associated with linear fit of transformed data

stat.XReg

List of data points in the modified X List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.YReg

List of data points in the modified Y List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.FreqReg

List of frequencies corresponding to stat.XReg and stat.YReg

Local

Local Var1[, Var2] [, Var3] ...

Declares the specified vars as local variables. Those variables exist only during evaluation of a function and are deleted when the function finishes execution.

Note: Local variables save memory because they only exist temporarily. Also, they do not disturb any existing global variable values. Local variables must be used for For loops and for temporarily saving values in a multi-line function since modifications on global variables are not allowed in a function.

Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook.

Lock

LockVar1[, Var2] [, Var3] ...
LockVar.

Locks the specified variables or variable group. Locked variables cannot be modified or deleted.

You cannot lock or unlock the system variable Ans, and you cannot lock the system variable groups stat. or tvm.

Note: The Lock command clears the Undo/Redo history when applied to unlocked variables.

See unLock, here, and getLockInfo(), here.

log()

log(Value1[,Value2]) value

log(List1[,Value2]) list


Returns the base-Value2 logarithm of the first argument.

Note: See also Log template, here.

For a list, returns the base-Value2 logarithm of the elements.

If the second argument is omitted, 10 is used as the base.


If complex format mode is Real:


If complex format mode is Rectangular:

log(squareMatrix1[,Value]) squareMatrix

Returns the matrix base-Value logarithm of squareMatrix1. This is not the same as calculating the base-Value logarithm of each element. For information about the calculation method, refer to cos().

squareMatrix1 must be diagonalizable. The result always contains floating-point numbers.

If the base argument is omitted, 10 is used as base.

In Radian angle mode and Rectangular complex format:

To see the entire result,
press 5 and then use 7 and 8 to move the cursor.

Logistic

Logistic X, Y[, [Freq] [, Category, Include]]

Computes the logistic regression y = (c/(1+ae-bx)) on lists X and Y with frequency Freq. A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension except for Include.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Category is a list of numeric or string category codes for the corresponding X and Y data.

Include is a list of one or more of the category codes. Only those data items whose category code is included in this list are included in the calculation.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.RegEqn

Regression equation: c/(1+ae-bx)

stat.a, stat.b, stat.c

Regression coefficients

stat.Resid

Residuals from the regression

stat.XReg

List of data points in the modified X List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.YReg

List of data points in the modified Y List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.FreqReg

List of frequencies corresponding to stat.XReg and stat.YReg

LogisticD

LogisticD X, Y [, [Iterations] , [Freq] [, Category, Include] ]

Computes the logistic regression y = (c/(1+ae-bx)+d) on lists X and Y with frequency Freq, using a specified number of Iterations. A summary of results is stored in the stat.results variable. (See here.)

All the lists must have equal dimension except for Include.

X and Y are lists of independent and dependent variables.

Freq is an optional list of frequency values. Each element in Freq specifies the frequency of occurrence for each corresponding X and Y data point. The default value is 1. All elements must be integers 0.

Category is a list of numeric or string category codes for the corresponding X and Y data.

Include is a list of one or more of the category codes. Only those data items whose category code is included in this list are included in the calculation.

For information on the effect of empty elements in a list, see “Empty (Void) Elements,” here.

 

Output variable

Description

stat.RegEqn

Regression equation: c/(1+ae-bx)+d)

stat.a, stat.b, stat.c, stat.d

Regression coefficients

stat.Resid

Residuals from the regression

stat.XReg

List of data points in the modified X List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.YReg

List of data points in the modified Y List actually used in the regression based on restrictions of Freq, Category List, and Include Categories

stat.FreqReg

List of frequencies corresponding to stat.XReg and stat.YReg

Loop

Loop
     Block
EndLoop

Repeatedly executes the statements in Block. Note that the loop will be executed endlessly, unless a Goto or Exit instruction is executed within Block.

Block is a sequence of statements separated with the “:” character.

Note for entering the example: For instructions on entering multi-line program and function definitions, refer to the Calculator section of your product guidebook.

LU

LU Matrix, lMatrix, uMatrix, pMatrix[,Tol]

Calculates the Doolittle LU (lower-upper) decomposition of a real or complex matrix. The lower triangular matrix is stored in lMatrix, the upper triangular matrix in uMatrix, and the permutation matrix (which describes the row swaps done during the calculation) in pMatrix.

lMatrixuMatrix = pMatrixmatrix

Optionally, any matrix element is treated as zero if its absolute value is less than Tol. This tolerance is used only if the matrix has floating-point entries and does not contain any symbolic variables that have not been assigned a value. Otherwise, Tol is ignored.

If you use or set the Auto or Approximate mode to Approximate, computations are done using floating-point arithmetic.
If Tol is omitted or not used, the default tolerance is calculated as:
5E-14max(dim(Matrix))rowNorm(Matrix)

The LU factorization algorithm uses partial pivoting with row interchanges.