| Module 24 - Vectors | ||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||
| Lesson 24.3: Projectile Motion | ||||||||||
|
It is useful to find a vector function that models the path of a projectile. Such a function can yield the particle's position at time t as well as it's velocity and acceleration. This lesson will explore finding the function that models the path of such an object given some initial information. Finding the Position Vector A projectile is fired from ground level. If the starting point for the projectile is considered to be the origin and if air resistance is neglected, the position vector for the projectile at time t is
where v0 is the initial velocity of the projectile,
The position vector can also be represented with the parametric equations
Exploring a Specific Example
Suppose a projectile is fired at an angle of
24.3.1 Use the trace key to approximate when the projectile reaches its highest point and the maximum height. Click here for the answer. Recalling Previous Functions If you have not cleared the variables r,v and a since Lesson 24.2, these variables should still be defined as the position, velocity and acceleration vectors for the parametric equations stored in xt1 and yt1. If you have cleared these variables, redefine them as they were defined in Lesson 24.2.
Verify that these functions have been updated with the new parametric equations
Notice the acceleration vector is 0i - 32j for all values of t because the only force acting on the projectile is gravity. Finding the Highest Point Find the vertical component of the velocity vector.
When the projectile reaches its highest point the vertical component of the velocity vector is zero. 24.3.2 Find when the projectile reaches it highest point by entering solve(v(t)[1,2] = 0, t) Click here for the answer. 24.3.3 Evaluate the position vector at the value of t that makes the vertical component of the velocity zero. Click here for the answer. |
||||||||||
| < Back | Next > | ||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||