| Module 17 - Applications of Integration | ||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||
| Lesson 17.3: Arc length | ||||||||||||||||||||
|
This lesson introduces the Arc Length Theorem and uses it's formula to compute the length of an arc of a curve. The lesson also explores using the TI-89's arc length feature, which is found in the Graph menu, and the arc length function, which is a built-in TI-89 function. The length of an arc of a section of a curve can be found by using an integral, as shown in the following theorem. Arc Length Theorem If a curve y = f(x) has a continuous derivative on the interval [a, b], its arc length is given by
Using the Theorem to Find Arc Length The theorem often gives integrals that are difficult or impossible to evaluate by hand. The TI-89 can be very helpful in evaluating or approximating these integrals. Find the length of the curve y = x2/3 on the interval [1, 2].
Keep the entry in the History Area for use later in this lesson.
The decimal approximation of the exact result is 1.16024 units. Using the Arc Length Feature There is an arc length feature in the Graph Math menu.
The calculator should prompt you for the first point, which is the left bound of the arc.
After pressing
After pressing
The answer matches the approximation found using the theorem. 17.3.1 Find the exact length of the curve y = x2 on the interval [-1, 2] and find a decimal approximation.
Click here for the answer.
17.3.2 Use the Arc feature of the Graph Math menu to approximate the arc length of y = x2 on the interval [-1, 2]. Compare the result with the answer found in Question 17.3.1. Using the arcLen Function
The arcLen function, which is found in the catalog or by pressing
This is the same answer obtained using the theorem at the beginning of this lesson. |
||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||