Module 17 - Answers
 
Lesson 1
 
 Answer 1
 
17.1.1  

   

The value of the integral over [0, ] where the area is above the x-axis, is 2. The value of the integral over [ ,2 ] where the area is below the x-axis, is -2. Therefore the net area over [0, 2 ] is 0.

 
 Answer 2
 
17.1.2  

The net area is square units, which is the sum of the two areas that lie above the x-axis minus the area that lies below the x-axis.

 
 Answer 3
 
17.1.3  

  1. The curve is decreasing on (0, 4), so the area function is concave downward on the interval.
  2. The curve is positive when x < 2 and negative when x > 2, so the area function has a maximum at x = 2.
  3. The curve appears to have equal areas above and below the x-axis on the interval, so the area function is 0 when x = 4.

A Net Area Function

 
Lesson 2
 
 Answer 1
 
17.2.1

The total area between f(x) = sin x and the x-axis between x = 0 and x = 2 is 4 square units.

 
 Answer 2
 
17.2.2

The TI-89 is not able to integrate , as indicated by the result being the same as the command.

However, the graph of y = x3 – 3x2 – x + 3 on the interval [0, 4] has two regions above the x-axis and one below.

The window is [0, 4] x [-5, 15].

After finding the zeros of the curve (x = 1 and x = 3), integrate the curve over the separate intervals (0, 1), (1, 3), and (3, 4) then add their absolute values.

The total area is square units.

 
 Answer 3
 
17.2.3  

The area between the curves is , or approximately 11.6821 square units.

 
Lesson 3
 
 Answer 1
 
17.3.1

The exact answer is , which is approximately 6.12573 units.

 
 Answer 2
 
17.3.2

The result is the same as the decimal approximation found in Question 17.3.1.

 
Self Test
 
 Answer 1
 
 
 Answer 2
 

One possible net area function is shown below.

 
 Answer 3
 
 
 Answer 4
 
 
 Answer 5
 
7.6404
 
 Answer 6
 
dx, so f(x) = tan x.
 
 

  ©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy