| Module 15 - Riemann Sums and the Definite Integral | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| Lesson 15.1: Right-hand Riemann Sums | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
In this lesson you will find the area of the region bounded by the graph of f(x) = x2, the vertical line
Getting a First Approximation Adding the areas of the four rectangles shown below can approximate the area under the curve. The rectangles are called right-hand rectangles because the upper-right-hand corner of each lies on the graph of f(x) = x2.
Finding the Width of Each Rectangle
The rectangles have equal widths along the x-axis that can be found by dividing the length of the interval by the number of rectangles. Using four rectangles over the interval [0, 1], the width of each rectangle shown is
The x-coordinate of each right-hand endpoint is found by repeatedly adding the fixed width,
Finding the Area
Because the upper-right-hand corner of each rectangle is on the curve, the height of each rectangle is determined by the function, and the heights are found by evaluating the function at the right-hand x-coordinates. For example, the x-coordinate at the right-hand edge of the third rectangle is
The area of each rectangle is found by multiplying the rectangle's width times the corresponding height. The total area under the curve is approximated by the sum of the areas of all the rectangles. 15.1.1 Approximate the area under the curve f(x) = x2 between x = 0 and x = 1 using four right-hand rectangles by completing the table below. Enter the right-hand x-coordinate and the corresponding y-coordinate for each rectangle, find each rectangle's width and height, and enter its area.
Click here for the answer. Finding a Better Approximation To find a better approximation you could subdivide the region into more rectangles, but it is more instructive to find a general procedure using an unspecified number of rectangles. The following table shows how to find the sum of n rectangular areas. Using n Rectangles
Let x = a be the left side of the region, let x = b be the right side of the region, and let f represent the function. The width of each of the n rectangles is given by
Study the table carefully. It will help you understand how to define an expression for finding the area of a general rectangle that will be used to find the sum of the rectangular areas.
Creating the Right-hand Area Function As shown in the previous table, each right-hand x-coordinate has the form a + kw, where k = 1, 2, 3, ..., n. The height of the corresponding rectangle has the form f(a + kw), and the area of the region is approximated by adding the areas of the rectangles, which is expressed as
The TI-89 has a sum function that will be used to define a new function r r s. This new function will accept the values of the endpoints of the interval [a, b] and the number of rectangles to be used, n, and return the total area of the right-hand rectangles that approximate the area under the curve defined by f(x).
The approximate areas returned by the function rrs are clearer if the results are given in decimals.
This is the same total area you found in the table using the four rectangles:
Using more Rectangles You can use this function to approximate the area when the region is divided into more rectangles. 15.1.2 Use the function rrs to approximate the area under f(x) = x2 over the interval [0,1] using 10 rectangles, 50 rectangles and 100 rectangles. Click here for the answer. Converging Sums
If we continue to evaluate r r s (0, 1, n) for larger values of n, the sums will appear to converge to a limiting value. Evaluate the limit of r r s as n approaches
The limit function is in the Calc menu and
The exact area under the curve f(x) = x2 over the interval [0,1] is the value of the limit,
Do not clear the memory or the History area of the functions you defined in this lesson so that they may be used in Lesson 15.2. 15.1.3 Evaluate r r s (0, 1, n) on the Home screen. What is the limit of this expression as n approaches infinity? Click here for the answer. |
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||