| Module 2 - Computer Algebra | ||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||
| Lesson 2.1: Numerical Calculations | ||||||||||||||||||||
|
In this lesson you will use the TI-89 computer algebra system to perform exact and approximate calculations.
Mode Settings Modes and their settings control how numbers, commands, and graphs are displayed and interpreted. The Mode dialog box is the place where you can change the mode settings.
You can go to different pages within the dialog box by pressing
The Exact/Approx Mode Setting The Exact/Approx setting determines the way calculations are carried out and how the results of those calculations are displayed. By default, the Exact/Approx setting is AUTO, but you can select two other settings: EXACT or APPROXIMATE. All three settings are discussed in this lesson. The EXACT Mode In EXACT mode, all values entered as part of an expression are considered to be exact, all computations are done using exact methods, and all results are displayed in exact form (using fractions, square roots, etc.). To select the EXACT mode,
You should be on the Home screen. Notice one of the current Mode settings shown on the Status Line under the Edit Line is EXACT.
Now you are ready to perform exact calculations. If you make mistakes while entering the following calculations, you can erase with the
Exact Calculations of Fractions
After you press
Treatment of Decimal Numbers in Exact Mode
Notice that the TI-89 treats the decimal fractions 0.123 and 0.5 as exact. Exact Calculations Involving Square Roots The next calculation involves the square root function, which is a second function above the multiplication key in the right column of keys.
The TI-89 returns
2.1.1 Find the exact value of
Radian Mode In the next calculation, you are going to find the value of a trig function. Your calculator should say "RAD" in the Status Line, indicating that you are in radian mode. Radian mode is one of the factory default settings selected when you reset to the factory setting in Lesson 1.1. If your calculator is not in radian mode, you can change the Angle setting to Radian on page 1 of the Mode dialog box. Exact Calculations with Trig Functions
The exact value of
2.1.2 Compute
The APPROXIMATE Mode To see the difference between EXACT and APPROXIMATE modes, set your calculator to APPROXIMATE mode and then repeat the above calculations. To change to APPROXIMATE mode,
Your calculator should say APPROX in the Status Line.
Repeat the three calculations you found in Exact mode:
The AUTO Mode AUTO is the other setting available in the Exact/Approx menu of the Mode dialog box. AUTO uses APPROXIMATE mode whenever the expression to be evaluated contains a decimal point. Otherwise, AUTO uses EXACT mode whenever possible. Certain higher order functions (e.g. "integrate" and "solve") may return APPROXIMATE results even if your entry does not contain a decimal point, but only when an EXACT answer cannot be found. Calculating an Exact Value in AUTO Mode
To find
The TI-89 returns
Calculating an Approximate Value in AUTO Mode
To calculate an approximate value of
The result is approximate because the entered expression contained a decimal point. Viewing Large Results
Compute 2100 by pressing
The TI-89 computer algebra system computes the exact answer, but the result is too big to fit on the screen, as indicated by the small arrow at the right of the result. To see the part of the result that is hidden,
Now the first part of result is hidden, as indicated by the small arrow shown at the left of the result.
Approximate Results Using
Another way to obtain an approximate result is to press
You should still have the expression 2^100 in the Edit Line.
![]() The approximate result is given in scientific notation.
Calculating log x
The last calculation in this lesson involves logarithms. The natural logarithm (ln) is a second function above the x-variable key, which is in the left column of keys. There is no dedicated key for the common logarithm (log), but it can be found in the catalog, which is an alphabetical listing of all the commands and functions available. Pressing
To find the value of log(25),
The result, which is exact, is expressed in terms of natural logarithms.
2.1.3 Find the exact and an approximate value of log(32). Click here for the answer. |
||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||