| Module 27 - Polar Functions | ||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||
| Lesson 27.3: Area Bounded by Polar Graphs | ||||||||||
|
Lesson 27.1 introduced polar coordinates and Lesson 27.2 investigated the graphs of polar equations. This lesson explores finding the area bounded by polar graphs. Finding the Area Bounded by Polar Graphs
The area of the region between the origin and the curve r = f(
This definite integral can be used to find the area of the region enclosed by the cardioid
The complete graph of this function is plotted using the interval
The integral may be evaluated on your TI-83.
The area enclosed by the cardioid is approximately 18.8496 square units. The exact area is 6
27.3.1 Find the area enclosed by the curve r = 2 on the interval
Finding the Area Between Two Polar Curves
The area bounded by two polar curves where
This definite integral can be used to find the area that lies inside the circle r = 1 and outside the cardioid r = 1 cos
First illustrate the area by graphing both curves.
The area inside the circle and outside the cardioid lies in the first and fourth quadrants. To find the area between the curves you need to know the points of intersection of the curves. The TI-83 can display coordinates in Polar form.
The first point of intersection occurs when
The second point of intersection occurs when
The two points of intersection are at
The definite integral that gives the area is
The area is approximately 1.215 square units.
27.3.2 Find the area of the region inside the circle r = 3 sin
|
||||||||||
| < Back | Next > | ||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||