| Module 27 - Polar Functions |
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test |
| Lesson 27.1: Polar Coordinates |
|
Polar coordinates are an alternative way of identifying points in a plane. They are useful in many applications. For certain types of regions and curves, working in polar coordinates is much easier than working with (x, y) coordinates. Polar coordinates will be explored in this lesson and you will learn how to convert points given in rectangular coordinates to polar coordinates and vice-versa. Defining Polar Coordinates When assigning rectangular coordinates (x, y) to a point P in the plane, x is the horizontal distance and y is the vertical distance from the origin O to the point P.
If polar coordinates (r,
Recall that there are an infinite number of angles that are coterminal with
Converting Rectangular Coordinates to Polar Coordinates The TI-83 has features that convert coordinates from rectangular to polar and vice-versa. Suppose you wish to find a value of r for the rectangular point (3, 2).
This item returns the value of the r polar coordinate for a point given in rectangular coordinates.
The distance from the origin O to the point (3, 2) is about 3.6056, so the polar coordinate r is about 3.6056.
A value of
The rectangular point (3, 2) is represented as approximately (3.61, 0.588) in polar coordinates. Because the calculator is in Radian mode, the angle measurement is given in radians.
27.1.1 If (r,
Converting from Polar to Rectangular Coordinates
27.1.2 Use the
Unlike polar coordinates, the rectangular coordinates for any given point in the plane are unique. |
| < Back | Next > |
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|