| Module 23 - Sequences and Series | ||||||||||||||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||||||||||||||
| Lesson 23.2: Series and Sequences of Partial Sums | ||||||||||||||||||||||||||||||||
|
This lesson explores series and partial sums of infinite series. Series are used in many applications including integration, approximation, and the solution of differential equations. These applications arise in many disciplines, especially physics and chemistry. Defining a Series A series, which is not a list of terms like a sequence, is the sum of the terms in a sequence. If the series has a finite number of terms, it is a simple matter to find the sum of the series by adding the terms. However, when the series has an infinite number of terms the summation is more complicated and the series may or may not have a finite sum. Defining Partial Sums A partial sum of an infinite series is the sum of a finite number of consecutive terms beginning with the first term. When working with infinite series, it is often helpful to examine the behavior of the partial sums.
Suppose an infinite sequence is defined by
The first four partial sums of the associated infinite series are computed below, where sk represents the sum of the first k terms of the sequence.
Each of the results shown above is a partial sum of the series
Defining the Sequence of Partial Sums of a Series
The partial sums of a series form a new sequence, which is denoted as {s1, s2, s3, s4,...}. For the series given above, the sequence of partial sums is
If the sequence of partial sums for an infinite series converges to a limit L, then the sum of the series is said to be L and the series is convergent. Otherwise, the infinite series does not have a sum and it is divergent. Finding Partial Sums of Series The TI-83's sum( function and the Sequence Graphing mode are useful tools in understanding the sequence of partial sums of series. Using the sum( Function Partial sums can be computed with the sum function and may be used to help explore whether or not an infinite series converges. If it is convergent, the partial sums can also help estimate the sum of the series.
Investigate whether
Beginning with Zero
Explore the partial sums of the series
This result is called the fifth partial sum because the first five terms corresponding to k = 0, 1, 2, 3, 4 were added.
23.2.1 Approximate the tenth partial sum of the infinite series
Graphing the Sequence of Partial Sums
The graph of the sequence of partial sums for the infinite series
Recall that n is the independent variable in Sequence Graphing mode and it can be entered using the
Each point of this graph represents a partial sum.
This should be the same value for the tenth partial sum that you computed earlier on the Home Screen.
23.2.2 The graph of the sequence of partial sums appears to level off. What does this suggest? Creating a Table of Values for the Partial Sums Make a table to show the partial sums.
The Ask Mode You can compute partial sums of your choosing by returning to the Table Setup dialog box and selecting the Ask mode.
The table provides further evidence that the series converges.
Tests for Convergence Both the graph and table for the series of partial sums give some evidence a series converges. However, analytic methods must be used to be certain that a series converges. You should consult a calculus text for descriptions of tests for convergence and divergence for infinite series.
23.2.3 The ratio test is an analytic test for convergence and it shows that the series being discussed,
|
||||||||||||||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||||||||||||||