| Module 23 - Answers |
| Lesson 1 |
| Answer 1 |
|
23.1.1
As n gets large the terms in the sequence get closer to zero. |
|
|
|
|
| Answer 2 |
|
23.1.2
The last several values appear to level off on the x-axis suggesting that
|
|
|
|
|
| Answer 3 |
|
23.1.3
The sequence appears to converge to approximately 2.7.
|
|
|
|
|
| Lesson 2 |
| Answer 1 |
|
23.2.1
s10
|
|
|
|
|
| Answer 2 |
| 23.2.2 The fact that the sequence of partial sums appears to level off suggests that the sequence of partial sums converges, which means the infinite series converges. Trying larger values for nMax may add more evidence for this conclusion, but it is impossible to be certain that an infinite series converges based on a graph or a table. |
|
|
|
|
| Answer 3 |
|
23.2.3
The graph and table of partial sums indicate that the series converges to approximately 10.5. |
|
|
|
|
| Answer 4 |
| 21.2.4 In the previous table the 26th and 51st partial sums were both approximately 10.5. So a reasonable estimate for the sum of the infinite series is 10.5. |
|
|
|
|
| Lesson 3 |
| Answer 1 |
|
23.3.1
This is the Fibonacci sequence. |
|
|
|
|
| Self Test |
| Answer 1 |
| 1, 1, 0.5, 0.1667, 0.04167, 0.008333, 0.001389, 0.0001984, 0.00002480, 0.000002756 |
| Answer 2 |
| 2.71828 |
| Answer 3 |
The sequence appears to converge to approximately 0.377. The actual value is
|
| Answer 4 |
| 0.3751; 0.3715; 0.3697 |
| Answer 5 |
The series appears to converge to approximately 2.71828. The exact value is e. |
| Answer 6 |
|
The sequence appears to converge to approximately 63.8. The exact value is 64. |
|
|
|
©Copyright 2007 All rights reserved. | Trademarks | Privacy Policy | Link Policy |