| Module 6 - Limit as x Approaches a | ||||||||||||||||||||
| Introduction | Lesson 1 | Lesson 2 | Lesson 3 | Self-Test | ||||||||||||||||||||
| Lesson 6.3: Limits Graphically, Numerically, and Algebraically | ||||||||||||||||||||
|
In this lesson you will use graphical and numerical methods to support algebraic conclusions about limits. The limit of a function may be estimated from a graph of the function or numerically from a table of function values. The Graphical Approach
Estimate
The fact that there is no value beside the y-coordinate shows that Y1 is undefined at x = 0. However, the limit as x approaches 0 of the function is defined because you can get as close to 1 as you want by letting x be close enough to 0. The limit can be illustrated by using the Trace feature.
The graph and displayed values provide evidence that when x is close to 0,
Numerical Approach
The Table feature of the TI-83 can be used to evaluate
In the ASK mode you can enter any value you choose for x in the table and the calculator will generate the corresponding y value for functions selected in the Y= editor.
The table provides numerical evidence that
The Sandwich Theorem
The Sandwich theorem is used in many calculus books to prove that
This argument is called the Sandwich Theorem because the values of sin(x)/x are "sandwiched" between the values of cos(x) and 1. Simultaneous Graphing The Sandwich theorem can be illustrated by graphing the three terms of the compound inequality simultaneously.
The simultaneous convergence of three graphs to 1 around x = 0 illustrates the Sandwich theorem's argument that
Redrawing the Graphs You can see the three functions converge again using the Clear Draw command.
Left- and Right-Hand Limits
The notation
The diagram illustrates the x-values approaching 0 through positive values and the corresponding values of
The notation
The diagram illustrates the x-values approaching 0 through negative values and the corresponding values of
Using the Trace Feature The Trace feature may be used to estimate these limits. As the Trace cursor moves along a curve, the x- and y-values appear at the bottom of the Graph screen.
Look at the y-values of
Moving the Trace cursor toward zero from the left and from the right provides graphical and numeric reinforcement for the left- and right-hand limits shown below. Entering a Specific x-Value While the Trace cursor is active, you can move it to a particular point by typing in the x-coordinate of the desired point. For example, move to the point with x = -0.001 while the Trace cursor is active.
The cursor is not visible because it is below the viewing window, but the coordinates of the cursor are shown giving further evidence that
|
||||||||||||||||||||
| < Back | Next > | ||||||||||||||||||||
|
©Copyright
2007 All rights reserved. |
Trademarks
|
Privacy Policy
|
Link Policy
|
||||||||||||||||||||