Transferring Files

To transfer files to or from the computer

1. Navigate to the FILE TRANSFER page.

2. Click either FROM CALCULATOR or TO CALCULATOR and follow the corresponding instructions below.

Note: Only .tns files can be transferred. Other file types will not be shown. Also, files on the calculator must be in the My Documents folder, not a sub folder.

 

File Transfer Troubleshooting

• Sending .tns files to and from nested folders on a calculator is not supported. The .tns file must be in the calculator My Documents folder in order to access the file.
• If a "Location not available." message appears when transferring .tns file to a computer or network location, this is because sending files to a location that contains system files is not supported (e.g. C:\, C:\Desktop, etc.). To avoid this, create a new folder or choose a different folder to transfer your files.