Student On-line Courses
TI-84 Plus CE -
![](/-/media/ti/education/images/resources/getting-started-with-ti-technology/aus/get-started-student-84plus-ce-hero-23271.jpg?rev=ce7d7dcd-d504-42aa-9a48-505262ac7c4d&la=en-AU&h=320&w=960&hash=69914460807C8AAEE74892300F441AEF)
Please fill out your name and answer all 10 questions.
The transformation graphing app is a great way to explore the transformative effect that variables can have on the graph of an equation. How many transformed equations and variables is it possible to examine at once?
How would I find where the vertical blue line (X1) intersects the diagonal black line?
Which of the following is not a possible way to find the median of a single variable data set on your calculator?
To force a decimal answer, which item would you select from the following menu:
What must you put around a Piecewise Function in the main screen when storing it as a y= function?
Where do we find the Application to solve polynomials as well as simultaneous equations?
The graph of y=x2 is shown on the screen in blue. The graph in red is a transformation of y=x2 which has been reflected about the x-axis, translated 3 units right and 4 units up. What would be the transformed equation entered into y2 in the y= editor?
What is the most efficient command to restore deleted lists? i.e. in this case L2, L3, & L5
In a Standard Window, when finding a Zero, rather than moving the cursor to find the Right Bound you can:
The quickest way to enter a fraction in MathPrint form is: