TI-Nspire Featured Activities Archive

Topic
  • Center and Spread

    Content Standard: HSS-ID.A.2

    Students will recognize that the mean and standard deviation (SD) and the median and interquartile range (IQR) are two ways to measure center and spread.

    Tootsie Pops & Hand Span

    Content Standard: HSS-ID.B.6a

    Students will collect data, find the linear regression model of the data, and address aspects of the data that affect regression.

    Extraneous Solutions

    Content Standard: HSA-REI.A.1

    Students will discover solutions of radical equations and investigate extraneous solutions. Students will find a solution algebraically and use technology to graphically find them.

    Linear-Quadratic Inequalities

    Content Standard: HSA-REI.D.12

    Students will use sliders to control the intersection of a quadratic and a linear inequality.

    Zeros of a Quadratic Function

    Content Standard: HSA-APR.B.3

    Students will use sliders to change the linear factors of a quadratic function. Students will connect the zeros of the quadratic function to the zeroes of the linear factors.

    Vertex and Factored Forms of the Quadratic Function

    Content Standard: HSF-IF.B.4

    Students will be able to identify and justify the effect of changing the parameters of a quadratic function in vertex form and factored form.

    Quadratic Functions and Stopping Distance

    Content Standard: HSA-REI.A.1

    Students will analyze and compare data for stopping distances for 3 conditions: normal conditions, talking on a cell phone, and a wet road.

    Finite Differences

    Content Standard: HSF-IF.A.3

    Students will investigate into the set of differences for linear, quadratic, and cubic functions.

    Linear Inequalities in two Variables

    Content Standard: HSA-REI.A.1

    Students will discover the basics of graphing a linear inequality.

    Applications of Linear Systems

    Content Standard: HSA-REI.C.6

    Students will use a system of linear inequalities to solve a problem a real world problem about parking cars and buses.

    Solving Systems by Graphing

    Content Standard: HSA-REI.C.6

    Students will compare a linear and an exponential relationship using both a spreadsheet and scatter plots.

    Comparing Linear and Exponential Functions

    Content Standard: HSF-LE.A.1a

    Students will compare a linear and an exponential relationship using both a spreadsheet and scatter plots.

    Trains in Motion

    Content Standard: HSF-BF.A.1a

    Students will visualize a solution to a system of equations and will explore a system that intersects in one point and identify the ordered pair that represents the solution.

    How Many Solutions to the System?

    Content Standard: HSF-IF.B.4

    Students will translate and rotate a line to visualize that a system of equations can have a unique solution, infinitely many solutions, or no solution.

    Multiple Representations

    Content Standard: HSF-IF.B.4

    Students will explore information represented in tables, graphs, and symbols to interpret the meaning of slope and intercepts in the context of a real world situation.

    Domain and Range

    Content Standard: HSF-IF.A.1

    This lesson involves identifying a set of x-values in both symbols and words, identifying the set of x-values used in generating the function as the domain of the function, and identifying the set of y-values used in generating the function as the range of the function.