A variable is a defined value that can be used multiple times in a problem. You can define a value or function as a variable within each application. Within a problem, variables are shared by TI‑Nspire™ applications. For example, you can create a variable in Calculator, and then use or modify it in Graphs & Geometry or Lists & Spreadsheet within the same problem.
Each variable has a name and a definition and the definition can be changed. When you change the definition, all occurrences of the variable in the problem are updated to use the new definition. In the TI‑Nspire™ software, a variable has four attributes:
| • | Name - User-defined name assigned when the variable is created. |
| • | Location - Variables are stored in memory. |
| • | Value - Number, text, mathematical expression, or function. |
| • | Type - Type of data that can be stored as a variable. |
Note: Variables created with the Local command within a user-defined function or program are not accessible outside that function or program.