You are here: Working with PublishView™ Documents > Using Zoom

Using Zoom

The zoom feature lets you zoom in on any object or area on the PublishView™ document for discussion, and zoom out to see an overview of the lesson. The zoom uses the center point of the viewable area to zoom in.

The default zoom setting is 100%.

To change the zoom percentage, do one of the following:
Type the number in the box and press Enter.
Use the - and + buttons to decrease or increase the percentage in 10% increments.
Use the drop-down arrow to choose a preset percentage.

The zoom settings are retained when you save the document.

 

© 2006 - 2016 Texas Instruments Incorporated