You are here: Working with PublishView™ Documents > Creating a New PublishView™ Document

Creating a New PublishView™ Document

1. From the Documents Workspace, click File > New PublishView™ Document.

—or—

Click , and then click New PublishView™ Document.

A blank letter-size document opens in the Documents Workspace. The orientation is portrait, which cannot be changed.
The default margin settings for the top and bottom margins are one-inch. There are no settings for side margins.
By default, a problem is added to the document.
By default, the document contains the page number in a # of # format at the bottom of the sheet.
The scroll bars on the right side of the screen and at the bottom of the screen are active.
2. Add TI‑Nspire™ applications and PublishView™ objects as needed to complete the document.

ClosedAbout PublishView™ Documents
ClosedExploring a PublishView™ Document
ClosedUsing the Status Bar in a PublishView™ Document

 

© 2006 - 2016 Texas Instruments Incorporated