You are here: Graphs Application > Graphing Scatter Plots

Graphing Scatter Plots

1. (Optional) Create two predefined list variables containing the x and y values to plot. You can use the Lists & Spreadsheet, Calculator, or Notes application to create the lists.

2. From the Graph Entry/Edit menu, select Scatter Plot.

Use the up and down arrow keys to move between the x and y fields.

3. Use one of the following methods to specify lists to plot as x and y.
- Click to select names of the predefined list variables.
- Type the names of the variables, such as v1.
- Type lists as comma-separated elements enclosed within brackets, for example: {1,2,3}.

4. Press Enter to plot the data, and then zoom the work area to view the plotted data.

 

© 2006 - 2016 Texas Instruments Incorporated